Part Number: TIOS101
Hi Team,
customer tested the OCP function with the below schematics and found the problem.
V+=24Vdc, Vcc=3.3V, output is PNP or NPN type loading.
The test result as below.
output type
OCP startup value
OCP recover vaule …
Part Number: TIOS101 Other Parts Discussed in Thread: TIOS102 , UCC27517 What does residual voltage mean for the TIOS101? We will be using it in push-pull mode. Does is means the output will not drive all the way to 0V when the input is high? We want to…
Part Number: TIOS101 Hi team,
The NFAULT behavior seems different from datasheet description. Could you give me your advice?
There is 400mA-500mA output current when they drive a relay unit. ILIM_ADJ is open. NFAULT is pulled up to 3.3V.
They expect NFAULT…
Part Number: TIOL1115 Other Parts Discussed in Thread: TIOS101
Hello,
My main application is to integrate the magnetic reed sensor switch to activate and deactivate the output which are pilot valves.
I had planned to connect the sensors directly to the…
Part Number: TIOS101
Hi Team,
I have a question about TIOS101 abso max ratings and driving inductive loads.
TIOS101 CQ pin abso max is ±65V(transient pulse width < 100us for VCC and OUT). "9.2.2.3 Driving Inductive Loads" mentions a significant…
Part Number: TIOS101 Hello, TOIS101 datasheet specifies "OUT pull-up/down current" as 50uA. My customer would like to know where this leakage current come from in the device to understand this device behavior. Could you please explain it?
Regards…
Part Number: TIOS101 Other Parts Discussed in Thread: TPS62088 , Hi all
My customer is working on a design with the TIOS101.
They are using an upfront DC-DC 24V => 5V and then the TPS62088 as 5V => 3.3V step-down to be provided to PIN 1(VCC_IN). …
Part Number: TIOS101 Hi all
My customer is evaluating the TIOS101 and they have below questions.
Please review and comment.
Best regards
Ueli
---------------------------------
9.2.2.3 Driving Inductive Loads
The datasheet states: This voltage is clamped…
Part Number: TIOS101 Dear team,
Happy new year!!!
My customer want to get PSpice model of TIOS101x. Is there PSpice model of TIOS101x?
If there is no model for PSpice, Is it possible to make PSpice model for TIOS101x?
Thank you.