Part Number: TIOS101 If the TIOS101 is powered, EN=high, and I toggle IN, should I expect a momentary 'short' of the power rails, due to both high-side and low-side switches transiently being "on"? Or is there an internal crossover protection…
Part Number: TIOS102 Other Parts Discussed in Thread: TIOS101 Tool/software: FROM SBEM PVT LTD
REQUEST FOR IBIS MODEL:
Required IBIS Model
For EMC analysis.
5 kHz to 10 kHz, 10 +/- 1.5 V, 5 mA load output drive.
Integrated Surge Protection Required.
Part Number: TIOS101 I am using the TIOS101 (no internal LDO) in a circuit where the VCC_IN can be un-powered and VCC pin can be powered or vice versa.
I noticed that when VCC_IN is un-powered and the VCC pin is powered (24V), the VCC_IN pin continually…
Part Number: TIOS101 I'd like to use the TIOS101 in a 24V-48V application.
The datasheet shows an absolute max rating on VCC and OUT of 55V, but a recommended max of only 36V. What is the reason for the wide difference in absolute vs recommended? …
Part Number: TIOS1013 hi,
We are doing functional as well as EMC testing for TIOS101-3 at the moment and hope that the performance of the TI chip meets requirements.
We have one particular issue at hand regarding immunity to transient surge voltage. If…
Part Number: TIOS101 Other Parts Discussed in Thread: TLV760
Hello Team,
in regards to the following info:
LDO output voltage across temperature
Output current vs. Input voltage (beside the thermal limitation that may apply)
Do we have the plot for…
Part Number: TIOS101 Hi,
I'm using TIOS101.
According to datasheet, Current can be limited by adjusting Rset.
And this seems to be possible regardless of PNP and NPN.
But in my opinion PNP is true, but not NPN.
Because PNP is current source, so current…
Part Number: TIOS101 Other Parts Discussed in Thread: TIOL111 Hello,
I have a temperature sensor (1wire) interface. Maxim part number DS18b20).I need to protect outputs with below scenarios. Do TI had any solutions to protect for below scenarios.
I have…
Part Number: TIOS101 Hello,
I'm going to use the TIOS101 (no-LDO version) a low-side driver only. From the datasheet and discussions in this forum, it looks like that the VCC pin shall be powered even the voltage is not passed to the OUT pin (as it would…
Part Number: TIOS101 Hello guys,
One of our customers is considering evaluating TIOS101 for their next products. But they are considering MAX14832 too.
MAX14832
https://datasheets.maximintegrated.com/en/ds/MAX14832.pdf
Could you please give me your answer…