Part Number: TIOS102 Other Parts Discussed in Thread: TIOS101 , TIOL112 Hello TI,
I'm designing with the TIOS102 and found an inconsistency in the datasheet ( www.ti.com/.../tios102.pdf) regarding the current limit setting.
…
Part Number: TIOS102 Hi,
We want to measure the lackage current for the output sinking current(low-side dirver) in PNP mode, and now, the current is about 10mA-40mA when there are no load, but it is 10uA in the datasheet.
We consider it is the error…
Part Number: TIOS102
I’m evaluating the TIOS102 for an application, and I need clarification on the device’s VCC(min) specification and how it relates to the internal P‑channel FET structure.
According to the datasheet, VCC(min) is 4.75 V . However…
Part Number: TIOS102 Hi,
We use the TIOS102 for the IO Link design, and now, we have below leakage current in reverse polarity issue;
We set the IN to 0V and set the EN to 3.3V, onnected the external power supply VCC-IN to the OUT pin through an…
Part Number: TIOS102 Tool/software: Hi team,
My customer plan to use TIOS102 (without LDO). I want to know if the IVCC below refers to the current consumption of 24V? Is it because of the internal LDO that causes the maximum static current of about…
Part Number: TIOS102 Other Parts Discussed in Thread: TIOS101 , Hello,
I'm interested in incorporating either the TIOS102 or TIOS1023 into an industrial sensor product I'm developing and would like to create simulations of this part in my system to…
Part Number: TIOS102 Other Parts Discussed in Thread: TIOS101 Tool/software: FROM SBEM PVT LTD
REQUEST FOR IBIS MODEL:
Required IBIS Model
For EMC analysis.
5 kHz to 10 kHz, 10 +/- 1.5 V, 5 mA load output drive.
Integrated Surge Protection Required…
Part Number: TIOS1023 Other Parts Discussed in Thread: TIOS102 , TIOL112 Tool/software: Dear team,
The customer want to know Absolute maximum rating of VCC_OUT for TIOS1023.
For TIOS102, Absolute maximum rating of VCC_IN is 6V like below. but we can…
Part Number: TIOS101 Other Parts Discussed in Thread: TIOS102 , UCC27517 What does residual voltage mean for the TIOS101? We will be using it in push-pull mode. Does is means the output will not drive all the way to 0V when the input is high? We want…
Part Number: TIOL112 Other Parts Discussed in Thread: TIOS102 Tool/software: Hello:
We are considering TIOL112 as a general purpose DIO for a DAQ (24V capable). Do you see any issues with this approach? The thought here is to have one pin that can be…