Part Number: TIOS1023 Hi,
Before applying the TIOS1023 device to our project, we plan to perform circuit verification using PSpice simulation.
After reviewing the TI website and E2E Design Support resources, we were unable to find an available SPICE…
Part Number: TIOS1023 Tool/software: Team,
I would like to ask few questions about the TIOS102x chip specifications.
From the datasheet:-
“The VCC and OUT pins of the device are capable of withstanding up to 1.2 kV of 1.2/50 – 8/20 μs IEC 61000…
Part Number: TIOS1023 Tool/software: Hi team,
If the 3.3V of the TIOS1023 chip is short-circuited, will the TIOS1023 chip be burned? If not, will the overheat protection be triggered? Please help confirm this.
Thanks
Lillian
Part Number: TIOS1023 Other Parts Discussed in Thread: TIOS102 , TIOL112 Tool/software: Dear team,
The customer want to know Absolute maximum rating of VCC_OUT for TIOS1023.
For TIOS102, Absolute maximum rating of VCC_IN is 6V like below. but we can…
Part Number: TIOS1023
Tool/software:
Dear team,
The customer are using TIOS1023 but there is some issue like below. please review it and let me know your opinion.
- TIOS1023 output waveform
=> NPN configuration , no load status. EN = Low
As…
Part Number: TIOS1023 Tool/software: Dear team,
My customer would like to use TIOS1023 as output driver for their application.
Main concern is thermal issue due to ultra small board size. so they would like to calculate power dissipation and the junction…
Part Number: TIOS1023 We have connected the NFAULT through a 10K PU to +24V VCC pin on TIOS1023.
Will the NFAULT pin tolerate this voltage given we adhere to the absolute maximum rating of NFAULT current being < 5mA?
Thanks!
Lev
Part Number: TIOS1023 So I have designed in the new TIOS1023 part and have come to the point of setting the current limit resistor.
Figure 6-4 in the datasheet gives a graph showing current limit vs the set current limit resistor.
Question 1 : Is…
Part Number: TIOS1013 Other Parts Discussed in Thread: TSM36A , TIOS1023 Dear TI Team,
We are experiencing a problem with Surge Test and the TIOS1013 chip. When we apply 1 kV Surge to the output pin, we get a 15 ms reset at the output. This must be…