Part Number: TL16C752C Tool/software: Hello Team,
My customer used 24MHz crystal as a clock source, but they need to change it to external 20MHz oscillator.
on datasheet, there's no comment on the XTAL1's operating range. is it ok to use 20MHz external…
Part Number: TL16C752C Tool/software: Nice to meet you.
I am currently developing using the TL16C752C.
I am developing with the communication settings set to no parity.
Sometimes, when I look at the Line Status Register (LSR), a parity error occurs…
Part Number: TL16C752C Tool/software: Hi all,
I would like to ask you NC pin.
TL16C752C Dual UART With 64-Byte FIFO datasheet (Rev. C)
The datasheet says' 'No internal connection'' about NC pin. It is necessary that NC pin is open?
I couldn…
Part Number: TL16C752C Other Parts Discussed in Thread: TL16C752D Tool/software: Hi team,
I have a customer with the below inquiry. Let me know your thoughts and thanks in advance!
"We are currently utilizing the Maxliner/Exar XR16L2750IM-F dual uart…
Part Number: TL16C752C Tool/software: Hi team,
I am running at 512kbps and it works fine when transmitting but gradually loses the INT signal when receiving. Are there any conditions under which the INT signal stops being generated? When the INT signal…
Part Number: TL16C752C Hello guys.
One of my customers uses TL16C752B for their current products using their stock of the device. But the stock will be run out in a few months. So they are evaluating TL16C752C for TL16C752B replacing.
In the evaluation…
Part Number: TL16C752C Hi,
Q1. What is the RXRDY Active Low transmission condition?
Q2. RXA/RXB receive and hold the UART, and when specified by A[2:0], CSA/CSB, and IOR, the function to output the corresponding 8bit of the held UART to D[7:0]. I…
Part Number: TL16C752C Hi,
The following procedure is used to check the operation using TL16C752C. However, we are unable to obtain the values as expected.
(1) A telegram (0xFF)(0x30)(0x30)(0x30)(0x30) is sent from the lower board every 500ms. Due…
Part Number: TL16C752C Other Parts Discussed in Thread: TMS320F28377D Hi all,
I`m using TL16C752C (Dual UART with 64-byte FIFO) as RS422 communication mode with EMIF.
However, due to my fault, the hardware was designed to receive more than 64 bytes…
Part Number: TL16C752C Hi,
Q1. I tried to change the value of register IER based on the timing chart in the data sheet, but the value read out was not changed from the initial value. Please check if the method of changing register IER is correct.
…