Part Number: TL16C752C Hi,
Q1. I tried to change the value of register IER based on the timing chart in the data sheet, but the value read out was not changed from the initial value. Please check if the method of changing register IER is correct.
…
Part Number: TL16C752C Hi Experts,
Good day. Seeking your assistance on this query:
Errata for TL16C752CPFBR suggests 2 work arounds. First is change number of stop bits to 1.5 or 2. Where do I make this change, at this device as a receiver, at the…
Part Number: TL16C752C Other Parts Discussed in Thread: TL16C752D Hi, I am currently using this 64 byte FIFO (TL16C752) with C6747 DSP. Currently I am using the FIFO to receive a periodic message of 26 bytes at 50Hz (20ms period). I have set an interrupt…
Part Number: TL16C752D-Q1 Other Parts Discussed in Thread: TL16C752CI-Q1 Dear team,
Does the SLLZ058A apply to C and D version or is there an updated errata for the D version? Could you pls also confirm that errata are valid for /Q1 and Q1 version…
Part Number: TL16C752C Hello Team;
I have question for IOW/IOR timing with CS signal to access.
Reference to Figure 1.General Write Timing on page 11(or Figure 2. General Read timing on page 12) of datasheet, IOR should be low while /CS=Low, Or, …
Part Number: TL16C752C Other Parts Discussed in Thread: TL16C752D Hello,
I have an old design using TL16C752B. The device is connected to a Ti DSP to provide two additional uarts both of which operate as 115k2 data pumps (i.e. no flow control) with…
Hi Satoshi
Yes, this is a typo (sorry for that) and yes, these devices are pin compatible.
Please, let me know if you have any questions.
Regards
Francisco
Part Number: TL16C752C Other Parts Discussed in Thread: TL16C752D
Hi all Would you mind if we ask TL16C752C? Our customer would like to use UART controller TL16C752C with following condtions; <Condition> Baud rate : 1200bps Rength to be transmitted…
Part Number: TL16C752C Hi all Would you mind if we ask TL16C752C? <Question1> On the datasheet P31, there is the description "IRQ Enable 0" on the MCR register bit3. Does it mean that this register indicates IRQ Enable and default status is "0"? <Question2…
Joe san We are looking for TL16C752C IBIS Model. It seems that 752c_rhb_5V.ibs is 754C model.(Our customer mentioned it.) Could you give us correct one? Kind regards, Hirotaka Matsumoto