Part Number: TL28L92 Hi,
We are looking to use the TL28L92 as a replacement for the SC28L92 and to that end have obtained some samples but have found that the TL28L92 does not work as advertised in our circuit.
We are using both channels where TXA is…
Part Number: TL28L92 We've used the TL28L92 to replace an obsolete NXP SC28L92 and found it works fine in 8-bit mode but does work in Multi-drop (9-bit) mode.
In Muti-drop (9-bit) mode the PARITY TYPE bit in Mode Register 1 determines the state of…
Part Number: TL28L92
We are facing an issue while transmitting data. As per data sheet, when the external clock is used by the transmitter in pin IP3, the transmitted data is clocked on the falling edge of the clock. But our transmit data when probed…
Part Number: TL28L92 Hi team,
Do we have sockets that can realize SPI to 2 channels UART?
I found TL28L92 can realize 2 channels, but its interface is X86.
Hi Mike,
I am on the gate drivers team. We have some similar-ish parts in the TPICxxx family that are multichannel drivers. However, they are all in SOIC type packages and none have 44 pins. Also, they are from the late 90's.
The only active part…
Hi Joe,
I don't know if TI is active working on this problem.
Maybe you can provide den HDL design and testbench under NDA? Then we could try to reproduce the error with a modified testbench and help you top fix the hardware bug.
Please help us to…