Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TL7700-SEP Hi team,
Quick question for you guys, on the TL7700-SEP datasheet is there a difference between the orderable part numbers, specifically:
TL7700CMPWPSEP vs V62/19602-01XE-T?
Or is it simply just a different orderable #.
Thanks…
Part Number: TL7700
Dear Technical Support Team,
Is it possible to use the datasheet specification(min/max) of Vs(Vcc=3V) for any Vcc voltage such as Vcc=5V within absolute max?
Datasheet has only Vs spec for Vcc=3V. So I'd like to know Vcc vs Vs specification…
Other Parts Discussed in Thread: TL7700 We have questions about TL7700.
Can we use this IC without capacitor of CT pin?
Please tell us the terminal processing of CT pin if we can use this IC without capacitor of CT pin.(Open or Connected to GND and so…
Part Number: TL7700 Other Parts Discussed in Thread: TPS3700
I posted it at the end of the following thread, but I also set up another thread just in case.
https://e2e.ti.com/support/power_management/supervisor_reset_ic/f/886/p/667726/2477836#247783…
Other Parts Discussed in Thread: TL7700 We have a question about TL7700.
Question 1.
Please tell us the reset time(min / typ / max) of TL7700.
We understand that reset time is the time from detecting overcurrent to reset signal output.
We want to know…
Part Number: TL7700 Hi,
We got a question from the customer about TL7700. Could you help us?
[Question] Are there any voltage level requirements between Vcc and Vs? They are concerned whether Vs voltage allows to exceed Vcc voltage, or not.
Best Regards…
Part Number: TL7700 Other Parts Discussed in Thread: TPS3840 , TPS3890 Hi,
We got a question from the customer about TL7700. Could you help us?
[Question] - How much is the variation of Vs at Vcc=1.8V, Ta=-40 to 85C?
- How much is the variation of Ict at…
Masumi,
I can't confirm the internal schematic you provided since I have not seen this before and it does not match what is provided in the datasheet. Since TL7700 is an open-collector output topology, a capacitor on the /RESET output so only affect…
Other Parts Discussed in Thread: TL7700 We have a question about TL7700.
Please tell us the voltage applied to the CT pin.
Voltage of CT pin doesn't depend on capacitance of CT.
we can calculate the voltage with the following formula.
Is this idea…