SHH,
We also have TL7700 which is a voltage supervisor with programmable delay and operates up to 40V. Please check the datasheet below.
www.ti.com/.../tl7700.pdf
-Michael
Part Number: TPS3808 Other Parts Discussed in Thread: TL7700 , UC1903 , TPS386000 Hi, team.
I received a question from the customer "Can we respond to negative voltage monitoring on TPS3808?" (The customer is considering of two ways.)
Can you tell…
Ronald san, We have one additional question. Our customer would like to make the output delay 30msec(tpo=30msec) using TL7700. -tpo = C t × 10(5) seconds So, Ct will be "3mF=3000uF". Is our recogniton correct? And then, is calculation formul…
Hello Robbie,
Once the interrupt has been cleared, set a flag and ask the main application to put it in Deep Sleep with lower power consumption setting.
There are similar products from TI like TL7700. Just go on to www.ti.com and search for voltage…
Other Parts Discussed in Thread: TL7700 I read the datasheet for TPS65381, it needs IGN signal, in datasheet "spna176",TL7700 is used to simulate IGN siganl ,but TL7700 operating temperature is 85°C,is there other similar IC can work under 100°C or above…
TL7700 output is an npn open-collector transistor, therefore, you can still drive the IGN to zero by a third ASIC.
Question: Suppose the TPS65381 goes to standy state, how can you wake it up? Sounds to me that you have to control IGN or CANWU pin. I think…
For currents less than 300mA, you can use the UC27131 smart power switch. For higher current you would need an external transistor to handle the power. You can also use a voltage supervisor such as the TL7700 or TL7712. You will need to invert the /RESET…
Hi,
I have a question regarding the power supply for TL7700CPWR.
I used this supervisory in the circuit for which I want to shut down the voltage regulator when the sense voltage goes below a certain threshold.
Can I connect the TL7700CPWR VCC to another…