Other Parts Discussed in Thread: TLC3578 Hello, all
Now we have one inquiry from our customer regarding VREFP supply voltage on TLC3578.
They are using LM4040BIM3-4.1 as reference supply into VREFP pin on TLC3578.
When referring other thread regarding this…
Hello Yoshida-san
It appears to be a settling related issue. The input voltage has to be transferred to the internal sample and hold capacitor, and incorrect non-linear (no gain/offset related) values could mean the source is high impedance. Is there…
Other Parts Discussed in Thread: REF5040 , TLC3578 Hi,
I am currently testing using the TLC3578IPW (TSSOP-24) on custom created board.
In this case i have pulled up the FS and CSTART as i dont have any dsp and all operations are to created using softwa…
Other Parts Discussed in Thread: TLC3578 , REF5040 Hi,
I am currently designing a circuit using TLC3578 where I have bipolar inputs of range +5V to -5V
In TLC3578 there is REFP REFM which are to connected as per datasheet via 3 capacitors
In the datasheet…
Other Parts Discussed in Thread: TLC3578 Hai
I am karthik. I am using TLC3578 to read single end voltages of range +5 to -5 Volt. I have used reference voltage of +4.096V at REFP and REFM is connected to AGND. I wanted to know am i right with the REFM…
Other Parts Discussed in Thread: TLC3578 I am using TLC3578 AD converter. In AD value to be gotten to read, Clock happens in AD Channel terminal, I want to know what is problem.
I will ask reply to mail. Kjk9blue.at.hotmail.com
Other Parts Discussed in Thread: TLC3578 hello, everybody! Recently ,I have been getting stuck with the communication between dsPIC33FJ64 and
TLC3578.I initialized and configured the TLC3578 according the TLC3578 datasheet,but it doesn't
work,always…
Other Parts Discussed in Thread: TLC3578 I am trying to code up an FPGA to communicate with the TLC3578 via Mode 00 or one-shot mode. Here is my problem, I write out the SPI code to select an analog input channel and wait for the conversion to complete…
Other Parts Discussed in Thread: TMS320C6416T , TLC3578
Environment: TMS320C6416T DSK + ADC TLC3578 + 5-6K Interface. Any sample code or any document based on the this data flow? I am writing the code for the connection but it doesn't work. I also looking…
Other Parts Discussed in Thread: TLC3578 , TLC2578 I have successfully interfaced the ADC to my controller, which will get input from a function generator (1V - 10V sine wave, 1 Hz - 1 MHz range),
the ADC will be used to display the voltage on a LCD. Now…