An example is the TLC6C598, it has a serial output to connect multiple LED drivers, and the DS says "The serial output clocks of the device on the falling edge of SRCK to provide additional hold time for cascaded applications"
Part Number: TLC6C598-Q1 Hello, Team,
The customer would like to know whether it is possible to input VCC + 0.1V to other signal lane pins.
Thanks and Best Regards, Masaru
Part Number: TLC6C598 Hi, Good day. I hope you are doing well. Our customer is using the TLC6C598 and they want to know if they can use the SPI from micro controller or GPIOs. I hope you could help us on this. Thank you. Regards, Cedrick
Part Number: TLC6C598-Q1 Other Parts Discussed in Thread: TLC6C598 Dear all.
Please review the circuit diagram of TLC6C598.
Three casades are connected as shown below.
In the second circuit, Pin no. 7&8 is connected by a 10 kohm resistance. Is this a…
Part Number: TLC6C598-Q1 Other Parts Discussed in Thread: TLC6C5912-Q1 , TLC6C5816-Q1 , Hi TI-team
Are TLC6C5816-Q1 or TLC6C5912-Q1 and cascade connection possible by this IC ?
Best Regards,
Koji Hayashi
Hi Michael,
TPIC6C595 will be EOL, so we don't recommend this device. TLC6C598-Q1 would be a recommendation.
But for this relay application, please add the clamp circuit on the output for protection.
The max clock frequency for SRCK is shown in the datasheet…
Part Number: TLC6C598 Other Parts Discussed in Thread: TLC59116-Q1 , TLC5917-Q1 , TLC6C5712-Q1 , TLC6C5724-Q1 , TLC5941-Q1 Hi Sir,
Does TI have similar ADDtek A701 6 Channel LED Driver?
http://www.yuketek.com/pdf/A701_702_B.pdf
Hugo
Part Number: TLC6C598 Hi team,
I would like to introduce TLC6C598 to drive LED indicator instead of discrete transistor solution.
But customer is worried about how much current can be used in total.
Could you confirm below conditions are ok or not and…
Part Number: TLC6C598 Hi, this is Takehira from Japan.
Please let me know about LED Driver TLC6C598's boot time.
How long (milli seconds) should I wait from power it on to input first signals such as SRCK for correctly operating?