Part Number: TLIN1024A-Q1 Tool/software: Hi team,
Could you provide storage condition spec "Tstg" for TLIN1024ARGYRQ1? The spec is not stated in Datasheet.
Regards,
Kento
Part Number: TLIN1024A-Q1
The max current including -45℃ and 125℃ temperature conditions is set at 20uA. (Vsup ≦ 14V)
Does the max current tend to decrease if only 25°C conditions? *The answer as a reference value (technical opinion) is fine.
Part Number: TLIN1024A-Q1 hi expert
Q1: if responder LIN VSUP is 7V, commander LIN VSUP is 12V, whether is it ok?
Q2:as we know, if LIN work as commander node, LIN bus need pullup resistor to power source. must this power source be same the VSUP?
(if power…
Part Number: TLIN1024A-Q1 Other Parts Discussed in Thread: TLIN1024-Q1
Hi,
My customer has a TLIN1024A-Q1 question. In 'high content' vehicles they use all the channels but on the 'low content' vehicles they only use two. What changes would need to occur…
Part Number: TLIN1024A-Q1 Other Parts Discussed in Thread: TLIN1021A-Q1 , TLIN1028-Q1 Hi team,
Any solution to have INH output for Device TLIN1024. I checked NXP device SJA1124 is having thta so replacement of SJA1124 will also work. We are doing new design…
Part Number: TLIN1024A-Q1 The proper connection of Vsup1/2 is confusing as the datasheet shows multiple ways to do that. The connections for the pullups for commander mode are also not clear.
- Figure 9-1 and Figure 12-1 show that Vsup1 and Vsup2 both…
Part Number: TLIN1024A-Q1 Other Parts Discussed in Thread: TCAN1046-Q1 , , TCAN1046A-Q1 Hi team,
Our customer is looking into the TLIN1024/TCAN1046 datasheet and it seems there are some difference in recommended schematics/layout.
For example in TLIN1024…
Part Number: TLIN1024A-Q1 Other Parts Discussed in Thread: TLIN1021A-Q1 Hi team
There is a good new that we could DIN TI product!
Customer is looking for the replacement of BD41030FJ-CGE2
https://fscdn.rohm.com/en/products/databook/datasheet/ic/interface…
Part Number: TLIN1024A-Q1 Other Parts Discussed in Thread: TLIN1021A-Q1 Hi team,
I have two questions on TLIN1021A-Q1&TLIN1024A-Q1 in design:
1. Can we leave LINx pin float if it is not used?
2. Can we put two 220nF cap in series near the Vsup pin…