Part Number: TLIN1028-Q1 Tool/software: Dear TI experts,
I can see several ISO standards in the datasheet of TLIN1028-Q1.
Can I get the certificates about each ISO standards?
1. ISO/DIS 17987 2. ISO 7637 3. ISO 10605 4. ISO 11452-4:2011
Please…
Part Number: TLIN1028-Q1 Dear TI experts,
My customer have a question about rising time of LIN communication.
Customer now test their product with external Lab.
During the test they have to measure rising time of LIN communication.
The time within…
Part Number: TLIN1028-Q1 Hi Team,
Could you support following customer questions?
Q1 Regarding tPWR, what are the values of MIN and TYP respectively?
As far as my understanding, t_pwr depends on Vsup capacitance value. Is it correct?
Q2 When…
Part Number: TLIN1028-Q1 Tool/software: Hi,
In case the LDO of the TLIN1028-Q1 in not required, due to -20dB/dec in the loop when no load is connected it seems the LDO output pin (Vcc) might be left floating, could you confirm if this is true or if…
Part Number: TLIN1028-Q1 Tool/software: We are looking for unencrypted SPICE model of TLIN1028 to validate the measurement reports through ANSYS EMC simulation. This will help us consider exact behavior of module rather than any approximations.
We already…
Part Number: TLIN1028-Q1 Tool/software: Hi,
We are simulating the impact of LIN filter on ESD pulses.
One of the requirement is to have ESD pulse of +/- 4kV, 330ohms, 150pF pulse on contact pin of LIN (unpowered condition).
Schematics:
We…
Part Number: TLIN1028-Q1 Tool/software: Dear TI experts,
Can I get reports of TLIN10285DDARQ1 regarding to ISO 17987-7 and IEC 62228 ?
My customer have to send these reports to their end customer.
Please check this issue. Thanks.
Best regards…
Part Number: TLIN1028-Q1 Hi,
The customer wants to use TLIN1028-Q1 for Automotive.
Does it support ASIL-A design?
If you have a guide document for ASIL-A design, please share it.
Part Number: TLIN1028-Q1 Tool/software: Dear TI experts,
My customer got a comment from their end customer about TLIN1028-Q1.
"Reset signals shall use hysteresis to prevent instability with slow rise or fall of the power rail."
I caanot find the…