Hello Danny,
Thank you for your answer.
Could you please send us some details about the test setup and condition of the test you have performed.
Maybe there are some think that we did not made correctly on the setup.
Also a test report will be welcomed…
Part Number: TLIN1431-Q1 Tool/software: Hi Team,
I found the GENERIC PACKAGE VIEW and the PACKAGE OUTLINE are not aligned in datasheet. Could you please clarify which bottom pad should we refer?
Thanks
Best,
Frank
Part Number: TLIN1431-Q1 Tool/software: Would connecting this pin directly to the uC pin (Renesas RL78F24) without any additional HW start the controller in SPI or PIN mode?
Part Number: TLIN1431-Q1 Tool/software: We are using TLIN14315 SBC in one of our project. In this project we are facing issue with sleep and wakeup of our device. In our testing we found that device wakes up after going to sleep (around 200ms after sleep…
Part Number: TLIN1431-Q1 Hi, is there any sample code available for TLIN1431x ?? Any initialization code or other ? Is there ref design that uses it that we could borrow code from that ?
thanks,
JJ
Part Number: TLIN1431-Q1 Hi TI,
I am using TLIN14315-Q1, and VCC pin is 5V.
I have 470ohm + 100nF on VBAT pin, and 100ohm+100nF between PV pin and MCU ADC pin.
Then I provide VBAT=12.8V but measure PV pin is 1.42V. The ratio is around 1:9.
I think it should…
Part Number: TLIN1431-Q1 Hello,
I plan to use TLIN 1431 to supply a ECU with NXP microcontroller.
I wonder how can I start programming an uC (without software inside) .
My concern is that the watchdog will trigger a reset if the uC will not trigger it…
Dongwon,
Dongwon Kim said: <Q1> I would like to know if there is any difference in behaviour between the different settings of FSM_CONFIG below.
- 000b = Disabled
- 0010b = Perform soft reset
- 0011b = Perform hard reset - POR
Soft reset and hard…
Part Number: TLIN1431-Q1 I am currently working on a project with TLIN1431 SBC from TI.
Because of ASIL requirements we have enabled CRC mode for the SPI communication CRC_CNTL Ah address bit 0: CRC_EN set to 1 during the initialization phase.
During…
Part Number: TLIN1431-Q1 Hello,
I am using the TLIN1431 part in our project and noticed a strange behavior: if the watchdog is not serviced after the initial configuration the SBC will also cut the VCC after 16 watchdog resets
The only register that…