OK... Perhaps one of the 32 subscribers to this forum post may be able to answer a question or two... So, here we go.
(There's a pretty graph at the end....)
Questions:
Is the DSA test done from one end only? Ie the far end PHY doesn't need to be…
Eirik,
Do you have a schematic that you can share? We are a little confused between : oscillator vs crystal? Are you using crystal? Because oscillator only gets connected to XI and not XO?
Also from the diagram shared above, can you share the waveform…
Part Number: TLK100 Hi I'm Jieun,
I have a question about PHY transceiver,TLK100.
According to the datasheet, Wrong polarity affects the 10B-T PHYs. 100B-TX is invulnerable to polarity problems because it uses MLT3 encoding.
Can I ask the reason…
Part Number: TLK100 Hello Support team,
My customer inquires evaluation result in application note SLLA310. Could you support?
*Is fig 10 - 11 result actual measured result? or simulation data? If simulation, which simulator this used?
*Can same eye…
Part Number: TLK100 Hi.
I'm going to use TLK100 with 3.3V power only.
How much current can V18_PFBOUT(pin number 40) output ?
I want to connect logic ic power(LV14 or LV2G) only. Is this no problem ?
Best regards.
Part Number: DP83848I Other Parts Discussed in Thread: TLK100 Hi Experts,
can we give some guidance how to migrate from the TLK100 to DP83848I?
they are not pin compatible but is there an overview available what changes are necessary in the registers and…
Part Number: TLK100 Other Parts Discussed in Thread: DP83826E , DP83822I , DP83825I Dear team,
Any product to recommend to replace TLK100 as I see it was no longer recommend in new design?
Thanks.
Best regards,
Sammi
Part Number: DP83822I Other Parts Discussed in Thread: TLK100 , AM623 Hi TI Team,
We have an query on ethernet PHY, in the legacy design we have PHY TLK100 design supporting 10baseT/100baseTX.
We had used it as MII interface, output connected to external…
Part Number: TLK100 Other Parts Discussed in Thread: TIDA-00299 , TLK110 Hi Team,
My customer plan use TLK100 application EtherCat but have some question need you help.
1) Driver support or sample code?
Looks website have C code but data is empty. Could…