Part Number: TLK10022 Hi,
we have designed a data aggregator using 5 TLK10022 which we connect to an FPGA (Xilinx Ultrascale). We are having problems reading the information coming from the TLK's (basically we don't get anything). We have checked the…
Part Number: TLK10022 Other Parts Discussed in Thread: CDCE62005 , TLK10232 HI Sir
We would like to design HDMI to SFP+ and SFP+ to HDMI
1. May I know TLK10022 support this application ?
2. below structure have a CDCE62005 connect TX and RX at the same…
Part Number: TLK10022 Hi,
I would like to check availability of 10.24Gbps(2.56X4ch).
I know it can be supported upto 10Gbps.
I was wondering it is possible to change some parameter setting for 10.24Gbps.
please let me know 10.24Gbps transfering is possible…
Other Parts Discussed in Thread: TLK10022 , TLK10232 Hello,
We have a question regarding the datasheet for the TLK10022 at this link: http://www.ti.com/lit/ds/symlink/tlk10022.pdf
In reference to table 6-42 - RX Search Marker Character (Default 10'h27C…
Other Parts Discussed in Thread: TLK10022 , TLK10002 , CDCM6208 Hi,
I want to use two TLK10022 in two boards and delivery 10G signal. But I don't know how to design the REFCLK. I see in a ducoment in TI website named"tidu689.pdf", the test report likes…
Other Parts Discussed in Thread: TLK10022 Our customer has this question:
We have the TLK10022 part configured in 4 lane mode, but we only have 1 2.5Gbps lane connected to the INBP/N0 input of the chip.
Will the part be able to recognize that only 1 lane…
Other Parts Discussed in Thread: TLK10022 Hi:
I want to use 2 TLK10022s between two boards A and B like the picture below.My questions is,how could I make sure the OUTBs be the same as the INAs? The refenrece clocks in these two boards need specially…
Hi Nan,
I was able to create a good method for generating data similar to what the customer might have in their system. Essentially I made a script for converting 8b data (which is what is referenced in slvs-ec specification) into 10b encoded data, which…
Other Parts Discussed in Thread: TLK10022 Hello!
Normally one would use two TLK10022 to combine and decombine some high speed signals in order to reduce the number of lines required. But we would like to use just one TLK10022 to combine four digital signals…
Other Parts Discussed in Thread: TLK10022 Hello,
Following is my system block and my purpose is to use TLK10022 to mux four independent 2.5Gbps LS into one 10Gbps,then back to FPGA.
PRBS15 generator and checker in FPGA will calculate BER of four channel…