Other Parts Discussed in Thread: TLK10022 Hello,
Can TLK10022 transmit MADI ( Multichannel Audio Digital Interface) data ? Should it be possible? Thank you.
BR
Patrick
Other Parts Discussed in Thread: TLK10022 Hello, I'd like to ask about configuration of TLK10022; 1.My Application: The low speed side is connected to Aurora of Spartan-6 (4 lanes) 1) mode 4:1; 2) data rates of Low Speed is 2.5Gbps , High Speed is 10G…
Hi, Dylan !!!, Thanks for your support and Happy New Year !!
I am updating my question now, Please focus more this posting than previous one.
We are testing TLK10022 with electrical loop back connection.
Our test environment is .....
[DVI Port out, 148Mhz…
Part Number: TLK6002 Other Parts Discussed in Thread: CDCM6208 , TLK10022 Sir
I want to use reference clock that supports ARS mode in TLK6002.
Can i use CDM6208 CDCM6208 2:8 Clock Generator, Jitter Cleaner With Fractional Dividers?
Pls suggest me
I have…
Hi,
Based on your description I'm not sure whether any TI part number cleanly fits the desired function. My recommendation would be to consider the following part numbers.
TLK10022
https://www.ti.com/product/TLK10022
TLK2501 or TLK2711-SP
https…
Hi,
Unfortunately, with further investigation this application TLK10031 will not work. When using SGMII there is no 8b/10b encoding of the data and the device will not be able to aggregate and serialize the data correctly. If you are able to use 8b…
Hi,
Unfortunately, with further investigation this application TLK10031 will not work. When using SGMII there is no 8b/10b encoding of the data and the device will not be able to aggregate and serialize the data correctly. If you are able to use 8b…
Part Number: TLK10002 Other Parts Discussed in Thread: TLK10022 We are going to use the TLK1002 to perform the serialization / deserialization of the TMDS lines of an HDMI / DVI signal, b ut have a few questions :
1. The Clocking examples of the TLK10022…
Other Parts Discussed in Thread: TLK10232 , TLK10022 Hi Team do you have the PCIE to LAN solution as the following block diagram? similar part: BCM957304A3040C
Thanks, SHH