Part Number: TLK10031 Hi Team,
We understand that the default setting of TLK10031 when MODE_SEL pin held low is 10GKR/1G-KX mode.
If we use 10G-KR and don’t use detail setting, can TLK10031 operate even if we don’t set the register by MDC and MDIO?…
Part Number: TLK10031 Hello,
We are using the TLK10031 to convert from XAUI to 10GBASE-KR. The below figure shows the data flow path in our design:
SWITCH <-------------> TLK10031(LS)<------------>TLK10031(HS) <------------> SFP+
XAUI …
Part Number: TLK10031 I wonder if you could help me with an issue I'm seeing accessing some of registers in the TLK10031 - when operating in Clause 45 MDIO mode.
We are using the TLK10031 to convert from XAUI to XFI (10GBASE-R). We have a Marvell…
Part Number: TLK10031 HI Sir
I use one TLK10031 to do the TX (transceiver) and one TLK10031 to do the RX (receiver)
So far we meet link error issue (FPGA have link error count) ,Please kindly help
Result
1. Use 10G LR Fiber module + 10KM fiber cable…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 , Hi team,
My customer has used TLK10232 for their system and is just looking for 1ch XAUI to 10G-KR SerDes device.
My customer would like to know the difference between TLK10232 and TLK10031…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232 , Hello team,
Is the TLK10031 pin to pin compatible with the TLK10232? If so, how I could to connect it to replace the TLK10232 with the TLK10031 is I am using just CHA?
Thanks in advance…
Hi Brian,
On the low-speed side, register 0x0008 bits 11:8 are the only way to check RX adaptive equalization settings. Here is a short document which explains how each of the adaptive EQ settings work.
TLK10031-034-232_LS_EQ Details.doc
On the high…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10034 I wonder if you could provide any help with an issue we're having using the TLK10031 to perform XAUI to XFI (10GBase-R) translation/converstion as per section 8.1 in the datasheet (-see…
Part Number: TLK10081 Other Parts Discussed in Thread: DP83869HM , DP83869 , TLK10022 , TLK10034 , TLK10232 , TLK10031 Hi, I'm working on an application that aggregates 2 gigabit ethernet into a single high-speed link bidirectionally like this:
(LS) 2 x…
Part Number: TLK10031 Other Parts Discussed in Thread: TLK10232EVM Hi Luis-san,
Our customer don’t use the following pins.
-LOSA (E9 pin)
-LS_OK_OUT_A (D9 pin)
-PRBSEN (B9 pin)
-PRBS_PASS (J9 pin)
Then, I understand that they can open the unused…