Part Number: TLK10232 Hi,
We have used TLK10232 device in one of our design as a XAUI to 10G-KR Converter plus cross-point switch.
Refer to the attached diagram for a high level view of the system.
tlk10232 Block Diagram.jpg
REFCLK used is 156…
Part Number: TLK10232 Hello,
For a project, I am using the TLK10232 to establish a 10GB Ethernet connection between a 10GB-KR switch (LAN9694) (channel A) and an Nvidia Jetson AGX Orin in XFI (channel B).
I am using the smart switch to connect the…
Part Number: TLK10232 Tool/software: Hi,
We are continuing to verify.
>Two TLK10232s are being used - did you use the loopback module to test the activity of both TLK10232s by themselves, if such a method was physically possible? The problem only…
Part Number: TLK10232
Hi team,
My customer plans to use TLK10232 as a ethernet PHY for 1GBase-KX, and connections are below.
Microcontroller <-> TLK10232 <-1GBase-KX-> Interface IC
In this use case, what is the interface of microcontroller connected…
Part Number: TLK10232 Other Parts Discussed in Thread: TLK6002 , USB-2-MDIO , MSP-EXP430F5529LP Hello,
For a large project, we are using several Orin AGXs interconnected (on the same card) via a switch. Between each Orin and the switch, we are using…
Part Number: TLK10232 Tool/software: Hello.
I am testing the TLK10232 by connecting it as shown below.
I am monitoring the following registers:
・CHANNEL_STATUS_1
・PMA_STATUS_1
・PMA_STATUS_2
・PCS_STATUS_1
・PCS_STATUS_2
・KR_PCS_STATUS_2…
Part Number: TLK10232EVM Other Parts Discussed in Thread: TLK10232 , TEST2 We are seeking your support with an unresolved issue using the TLK10232.
Summary:
Setup: TLK10232 EVM connected to our FPGA-based tester board via optical link
Test1 (EVM…
Part Number: TLK10232 Hello,
I have a board with TLK10232 connected to CX4 connector for XAUI transfer on the LS side and to SFP+ on the HS side.
I'm using BIDI SFP+.
I connect two boards together using the optical link and perform electrical loopback…
Part Number: TLK10232EVM Other Parts Discussed in Thread: TLK10232 , TEST2 RE_ TI Support for HP Israel.msg
We are seeking your support with an unresolved issue using the TLK10232.
Summary:
Setup: TLK10232 EVM connected to our FPGA-based tester…