Part Number: TLK10232 Hi Sir
I would like to use EVM to test loopback
Could you kindly help to provide a simple step up and process guide ?
Due to so far we test loopback ,have a lot of error message
Thanks
Hi Malik,
Sorry for the delay response. In our customised board we can able to achieve only 4Gbps in TCP. we are using Isola I - SPEED material for 10G Interface. Approximately 2 inches of trace between TLK10232 IC and SPF+ optical module cage.
Any…
Part Number: DP83869HM Other Parts Discussed in Thread: TLK10232 , DP83869 Hello,
We are considering the following design approach for i.MX8MP to work for a 1000Base-kx.
This approach involves two ICs. The first IC (PN: DP83869HM) is tasked with converting…
Part Number: TLK10232 Hi,ti
please answer following question,thank you!
1,If TLK10232 is as default hardware configuration and not configred by smi bus,can it work well and support xaui to sfi ?
2,If I connect TLK10232 to FPGA,the low speed bus of tlk10232…
Part Number: TLK10232 Hi,TI
I have some questions.
1,In my case,if I design the TLK10232 as default hardware configuration based on datasheet and it isn't configured by SMI bus,
the device can operation supporting xaui to sfi and support 10G SFP…
Part Number: TLK10232 I use 1gbit/s sfp module and configure it to send traffic but could not receive output clock (156.25 MHz) from channel A
device_addr 0x1e, addr 0xf 0x1403
device_addr 0x1e, addr 0x10 0x0 device_addr 0x1e, addr 0xd 0x2f80 possible problem…
Part Number: TLK10232 Hi Team,
Please allow me to clarify how to treat the pins when REFCLK is unused.
The datasheet says, "This input signal must be AC coupled. If unused, REFCLK1P/N should be pulled down to GND through a shared 100 ohm resistor…
Part Number: TLK10232
Hi Team,
As you know , there are 2 port in TLK10232.
I know that TLK10232 is reqired cofigulation.
And I'm writing following address , data to both port.
*Disable auto-negotiation by writing 1'b0 to 0x07.0000 bit 12 …
Hi Luis-san,
This thread has still been opening and I got a remainder on this from my customer.
They want to know TLK10232's "TI" shown in the figure above to fix MIDO read timing. Could you ask the parameter to designer ASAP if the Tvalid and T1 is…
Hi Malik
Please kindly help to check my question ,May I know your idea?
1. Yes!! We follow your test step ,we can measure the 100ohm on HSRX pin ,but in this moment we use differential probe to measure the HSRX pin's waveform
the eye amplitude is…