Hi Jayshree:
Jayshree Rapha said: Is it recommended to have 10K pull up on all TXD lines?
If TXD is not used, it's better to pullup or pulldown TXD pin.
Jayshree Rapha said: Are any series resistors recommended on any pins?
no series resistors…
Part Number: TLK2711EVM-CVAL Tool/software: Hello.
EVM board has pull-up, while device has internal pull-down at PRBSEN.
If EVM board Jumper does not installed, PRBSEN voltage is 1.7V.
( 2.5 V * 10k / (4.7k + 10k) )
Intermediate voltage is not…
Part Number: TLK2711EVM-CVAL Hi,
in my project I'm working with a TLK2711 so I'm interested in the EVM. Does the EVM include a cable for DC supply? if not, which kind of connector uses the EVM for the DC supply?
Thanks!
Part Number: TLK2711EVM-CVAL Other Parts Discussed in Thread: TLK2711-SP Hi,
I'm working in a project that requires use the TLK2711 (TX). The FPGA (RX) selected is the XCKU060 Kintex UltraScale and we are going to connect the TLK2711 with the GTH transceivers…
Part Number: TLK2711EVM-CVAL Hi TI,
For these eval schematics is there a BOM? Or at the very least a value for L1 and L3? The supply filtering for VDDA1 is aggressive and we want to match it.
Part Number: TLK2711EVM-CVAL Other Parts Discussed in Thread: TLK2711-SP Hi
We are using TI obsolete parts TLK2711IRCP transceivers
We purchased TI Evaluation board TLK2711EVM-CVAL (the EVB comes with TLK2711HFG transceiver on it)
We would like…
Part Number: TLK2711-SP Hi TI,
I found the figures below in this thread: https://e2e.ti.com/support/legacy_forums/hirel/f/space-high-reliability-forum-read-only/719646/tlk2711-sp-request-the-layout-lead-forming-data
The question I have is: Why is…
Part Number: TLK2711EVM-CVAL Hi,
We are doing the interoperability test between TLK2711 and Microchip RTG4 FPGA devices. Here we aim to send the PRBS-7 pattern at data rate of 2.5 Gbps from TLK2711 TX to RTG4 RX and through far end loopback send it…