Part Number: TLV320AIC24K My basic idea is to use a powerful dual core ARM processor to implement an audio digital delay using a CODEC chip connected to the processor where the incoming data is stored in the processor's internal RAM and then fed back…
Part Number: TLV320AIC24K Other Parts Discussed in Thread: LM49350 Hi
I want to use PCM interface to send digital audio from Tlv320aic24k to dsp and Bluetooth.
So can we use single PCM interface for two device ?
Part Number: TLV320AIC24K Other Parts Discussed in Thread: TLV320AIC23B Hi there,
With regards to the TLV320AIC24KIPFBG4 we have two questions with regards to the I2C interface.
On the datasheet the Rise time (t r ) of both SDA and SCL signals is specified…
Part Number: TLV320AIC24K Tool/software: Linux Is possible to create codec driver for current BBG kernel version ? I can not find example driver. How to create AIC24K codec driver ? or Do you have Example file for same family codec driver ?
Thank you. …
Part Number: TLV320AIC24K Hello,
I would like to use the hardware power down feature of the codec. Would you please tell me what happens to the digital I/O pins when PWRDN is pulled low.
I'm particularly concerned with FS, SCLK, FSD and DIN.
The…
Thanks a lot for there reply. I would like to split the question into 2 parts.
1.) You mentioned, that the default Processing Blocks cause a delay of ~2.1 - 5ms -> How can I reduce this? I need a reduction to delay <1ms for this part.
No processing…
Part Number: TLV320AIC24K Tool/software: Linux Is possible to create codec driver for current BBG kernel version ? I can not find example driver. How to create AIC24K codec driver ? or Do you have Example file for same family codec driver ?
Thank you. …
Part Number: TLV320AIC24K This is my first time designing with a TI CODEC, and I cannot get this puppy to work.
I have four TLV320AIC24K CODECs on my board. The first CODEC is wired to be the master (pin 21 pulled to IOVDD), and the other three wired…
Part Number: TLV320AIC24K We have this codec and are setting up the I2C port. Every time we read the control register status (using auto-increment of address), the value of register 3A toggles between our programmed value and 0x88. Also, control register…