Part Number: TLV320AIC3206EVM-U
Tool/software: AIC3206EVM GUI
I'm working with the AIC3206 EVM board Rev A.When I enable analog bypass from IN3_L/R to MAL/R to HPL/R – with a TRS microphone connected to J3-MIC IN and headphone connected to J5-HP OUT…
Part Number: TLV320AIC3206EVM-U Hello everybody!
I have some troubles with TLV320AIC3206EVM-U Evaluation Module. When i try to switch jumper W9 from 3.3V to 1.8V position i get 2.7V on IOVDD pin. Then i have removed W9 and W10 jumpers and measured voltage…
Part Number: TLV320AIC3206EVM-U Hi Experts,
Good day. Seeking assistance on this.
[1] It appears that the EVM for this chip (TLV320AIC3206EVM-U) doesn't have a simple way to test the digital microphones. Is that correct? If that is the case, I will…
Part Number: TLV320AIC3206EVM-U Hi Team, seeking your assistance.
Is there any document or file that is available regarding the dimension of the board?
Thank you.
-Mark
Hi,
I have a new question.
/1/ The Windows application for checking the operation of TLV320AIC3206EVM-U can be downloaded, but is there any software that can be used on a Linux PC (Ubuntu, etc.)?
/2/ Has the TLV320AIC32x4 i2c driver been proven…
Hi Avery,
There is no PPC3 for the AIC3206. Those scripts were written manually.
There is a control software for the EVM that can be downloaded from the EVM page. No request is required: https://www.ti.com/tool/TLV320AIC3206EVM-U
Best regards, Jeff…
Newer EVMs (~2007+)
The EVM User Guides for the devices below have been updated to include instructions on how to use these EVMs under Windows 7. Click a device, open the User Guide and search "Windows 7".
For the devices below, the EVM firmware must…
Hi Yordan,
Thank you very much for your help, we are still working on the issue which BeagleBone Black is not able to find the card.
I found the link( e2e.ti.com/.../1293890) , it seems that the following modules should be installed in order to solve…
How to revive a MC57xxPSIA board
The MC57xxPSIA is a board used to interface, configure and control the TAS57xx family of digital audio amplifiers.
The Firmware of the MC57xxPSIA may get corrupted, resulting in Windows not recognizing the board…