Hi,
Our customer evaluated bq27425 and took the SOC data like attached. Then they confirmed the abnormal SOC data at discharging and low battery voltage. Please let me know if you need more information to find problem in their test setup.
Best Regards…
Hi,
I am trying to install the following two images in the kernel with the bootargs,bootcmd as follows:
-rwxrwxrwx 1 mayank mayank 14327808 2011-08-27 16:05 cramfsImage_ipnc_DM368_IMX036 -rwxrwxrwx 1 mayank mayank 1865408 2011-08-27 15:57 uImage_ipnc_DM368_IMX036…
Other Parts Discussed in Thread: OMAPL138 , OMAP-L138 Team,
We performed some TCP testing on the OMAPL138. Our
objective is to get the Ethernet processing of an inbound TCP message under
100usec. In other words, Ethernet wire to application…
Hi Raghu/Anshuman,
Please help me on this issue.
I have seen your answers on e2e on dm368ipnc booting
and i need your help in making my board up.
I am trying to
install my uimage and cramfs image on the DM368-IPNC board but i…
Hi all,
I am trying to boot up the DM368IPNC board after installing my own uimage and cramfs built by using the procedure mentioned
in user guide.But when i am installing it on the board i am getting the following output and it gets stuck up…
Other Parts Discussed in Thread: TPS61220 , TPS61220EVM-319 Hello,
I've been doing some testing recently with the TPS61220 converter and I've noticed an interesting issue that isn't specifically mentioned in the component's datasheet. I apologize,…
Hello, there:
I am writing to ask for help about problems on running DSK6713 under CCSv5.5.0 (installed in Sept 2013) with Win7.
This is a re-post of the same problem to the CCS forum. An earlier post and follow up discussions can be found in the…
Hi,
Sorry for take so long to get back to you. Please apply the following 5 kernel patches onto the Processor SDK v6.2 kernel and let me know if the issue is solved.
Fullscreen
tiL4.19-P-v2-1-4-dmaengine-ti-k3-udma-Correct-completed-descriptor…
Edward, The C6748 LCDK does not have onboard JTAG emulation. To connect to Code Composer Studio running on a PC, you'll need to get a separate JTAG emulator. The relatively inexpensive XDS100 emulators lack the speed and features of the more expensive…