Hi Ian,
For higher PSRR please consider TLV702-Q1; however, it is important to note that these devices are not pin to pin compatible.
For part suggestions, keep in mind that the more information you can give us about how you are planning to use the…
Other Parts Discussed in Thread: TPS736-Q1 , TLV702-Q1 , LP5912-Q1 Hi,
I can see TPS73633-Q1 part in TPS736-Q1 Datasheet, I have TPS73633-Q1 (Fixed 3.3V output ) part, but I did not see TPS73633-Q1 order information.
Do you check TPS73633-Q1 RTM? can we provide…
Hi Ted,
Please excuse the short delay due to the US Holiday.
ESR requirements are set in order to help customers compensate the internal circuitry for a stable system. As each LDO part number is a different design, the compensation requirements may…
Ramgopal,
Your assessment of the bulk decoupling required is correct. You must calculate the required amount and validate it. The Hardware Design Guide (SPRABI2) discusses this calculation.
This bulk capacitance will affect the control loop on the power…
SI,
Please see the attached presentation. It was originally prepared for the LM10010 which was later superceded by the LM10011 which has higher precision. Please also see the many E2E posts discussing the LM10011 and TPS56121 with C667x and C665x.
To…