Other Parts Discussed in Thread: LP5907 , TLV707 I'm using TLV707 successfully and considering replacing it with LP5907 . They seem very similar. LP5907 has lower I[Q] and dropout.
What is the reason for making two parts that are so similar. Is the…
Part Number: AM5716 Other Parts Discussed in Thread: TLV707
Tool/software:
AM5716, customer is trying to switch to security-boot SOC
in the security boot document, what's the meaning of the temperature(junction)?
does it mean the junction…
Part Number: TPS7A05 Other Parts Discussed in Thread: TPS7A03 , TPS7A02 , TLV707 Tool/software: Dear Sir or Madam,
one question because I see in the datasheet follow description regarding the order code in chapter 11.1.2 Device Nomenclature:
Does…
Part Number: TLV707P Other Parts Discussed in Thread: TLV707 Hi Team,
customer is looking for TLV70728PDQNR.
They want to calculate/control the TLV707 series startup slew rate, can you help confirm the startup current?
Thanks!
Patty
Part Number: TPS7A02 Other Parts Discussed in Thread: TPS706 , , TLV707 Dear Tech support,
We have an application where we regulate the voltage from a rectifier circuit (NFC) to a large 11 mF 2.5V 'Super'-Capacitor meant to power a bluetooth IC for…
Hi Dong,
Unfortunately many of the LDOs only go to 0.5V outputs or higher. However you could use a resistor divider to further reduce this voltage.
For LDOs: A device like TLV707 which is a available in a 1mm x 1mm package (X2SON) with a 0.85V output…
Hi Harsh,
Please find the link below.
1. http://www.ti.com/product/LM5140-Q1/toolssoftware
2. http://www.ti.com/product/TLV707/toolssoftware
3. http://www.ti.com/product/TPS746/toolssoftware
4. Currently, the Pspcie model is not available. …
Hi Sundy,
I contacted our documentation group and they will add the mechanical dimensions and board land pattern to the datasheet.
For now, you can view the mechanicals in the TLV707 datasheet which has the same 1 x 1 mm DQN package:
www.ti.com…
Hi Kenneth,
16uF should be fine for TLV707. This device was developed targeting small mobile solutions. As such the majority of the characterization was done with smaller capacitors in order to minimize solution size.
We did not characterize TLV707…
Other Parts Discussed in Thread: TLV707 , LM317 Hello
In the datasheet for the TLV70730P version its explained that the P version has an active pull down circuitry on the output of 120 Ohm. This pull down resistor is it only active when the TLV707 is…