Part Number: TLVM23615 Tool/software: Hello,
It appears that the solder paste and land pattern shown in the datasheet and on the evaluation board are misaligned.
Also, in the footrprint generated by Ultra Librarian land pattern and solder paste…
Part Number: TLVM23615 Other Parts Discussed in Thread: LMQ66430 , Tool/software:
Hello, I'm having a problem with the TLVM 23615. I use this component to convert 24V to 5V and 3.3V to power CPUs. For 3 out of 5 boards I've had built don't work. 24V…
Part Number: TLVM23615 Hi Team,
I am using TLVM23615RDNR for 3.3V generation. Specs are as below
Input - 24V nominal
Output - 3.3V
At input series resistor of 22ohm and followed by two 4/7uF /50 V capacitors to input terminal.
When we powered…
Part Number: TLVM23615 Tool/software: Hello guys,
One of my customers is evaluating TLVM23615 for power supply with Vin=24V and Vo=1V.
The current datasheet says RFBT=10kohm and RFBB=10kohm for 1.0V output. But in case of these resistors, the output…
Part Number: TLVM23615 Tool/software: Dear Team,
My customer is considering to use the TLVM23615, and is looking at the datasheet of it. And they have a question about PG (PGOOD) rating. Can you please let me know the reason why the minimum spec of…
Part Number: TLVM23615 Tool/software: Hello guys,
One of my customers is considering using TLVM23615 for next products.
At this moment, they have the following question. Could you please give me your reply?
Q. Can TLVM23615 output (3.3V) be connected…
Part Number: TLVM23615 Tool/software: Hi Support Team,
We are currently evaluating a compact board using TLVM23615RDNR under the following conditions:
VIN: 24V
VOUT: 5.02V
IOUT: approx. 100mA
FSW: 1MHz (set via RT pin)
…
Part Number: TLVM23615 Other Parts Discussed in Thread: TPSM33625 Dear specialists,
My customer wants to simulate TLVM23615 with Webench.
The circuit was opened using the initial settings in WEBENCH.
When I try to select SIMULATE, the message "Simulation…