Part Number: TM4C1231H6PM TM4C team,
A customer is trying to access the SPI flash and having problems completing an erase. The SPI flash is 26F032B.
They tried operating in Mode 0, and weren't able to read or write.
They tried Mode 3, and they're able…
Part Number: TM4C1231H6PM Other Parts Discussed in Thread: UNIFLASH TM4C team or Tools team,
Is there a way to read the entire EEPROM contents using Uniflash or LMFlash Programmer, so you can write the contents to a second device?
Thanks, Darren
Part Number: TM4C1231H6PM
hi fellows,
when I have the AHB Bus enabled (GPIOHBCTL) I cannot see the register content in the Debug Mode and get the following error message.
CORTEX_M4_0: Trouble Reading Memory Block at 0x40025518 on Page 0 of Length 0x4…
Part Number: TM4C1231H6PM Hello Guys,
Greetings!
Access to I2C appears controller is busy . What are the reasons for I2CMCS to be triggered busy?
Is there anything that could be change in the register?
Looking forward to your response. Thank you in advance…
Part Number: TM4C1290NCPDT Other Parts Discussed in Thread: TM4C1231H6PM Copied working code from a project using a TM4C1231H6PM. Initialization code is:
SysTickIntRegister(SysTickISR); SysTickPeriodSet(GetClkSpeed()/100); // Interrupt every 10ms. (convert…
Part Number: TM4C1231H6PM
Hi,
Is it possible to cram a gpio output and an ADC input in the same pin? If seems possible from this block diagram from the spec sheet:
The ADC (red) is separated from the Pad input / output (blue) and that GPIODEN and GPIOAMSEL…
Part Number: TM4C1231H6PM Other Parts Discussed in Thread: TM4C123GH6PM , How do I configure pins PB2 and PB3 for PWM. Some of the pins that can be configured for PWM have M1PWM6 as a setting in the GPIOPCTL register. PB2 and PB3 just have timer.
Part Number: TM4C1231H6PM Hi,
If I have been stressing one particular region of the internal flash memory to more than 100k cycles, would it impact the performance of other regions of memory or just the region being stressed?
Thanks,
Jacky
Part Number: TM4C1231H6PM
Tool/software: TI C/C++ Compiler
I am trying to port a project from C to C++. At least during the transition, I would like to be able to compile it in either mode so I can compare performance, memory usage, etc. so I am trying…
Part Number: TM4C1231H6PM Tool/software: Code Composer Studio Multiple engineers are working on software. CCS version 6
They use the SD560.
When I build the project I get error:
Description Resource Path Location Type File connections/SD560V2USB_Connection…