Other Parts Discussed in Thread: TM4C123BH6PM Hi, I'm using an accelerometer(H3LIS331DL) to calculate position of an RC car with the Tiva MCU, TM4C123BH6PM.
I'm using SPI interface with the sensor.(2MHz SPI Clock) So far, reading the data is successful…
Other Parts Discussed in Thread: TRS3221 , MSP430F135 , MAX3232 Hello, I'm trying to connect my MCU to RS232 ports.
This is the schematic.
I'm not using EK or DK board. The DOUT, RIN is connected to the RS232 pins using a USB to serial cable.…
Part Number: TM4C123BE6PM Other Parts Discussed in Thread: TM4C123BH6PM Hi,
1. Is it correct to recognize that TM4C1231H6PMI is revision6 and TM4C1231H6PMI7 is revision7?
2. I would like to know if it is possible to replace the two devices in Question…
Part Number: TM4C123BE6PM Other Parts Discussed in Thread: TM4C123BH6PM ,
Hi,
We are considering replacing TM4C123BE6PMI7 (Flash: 126KB) to TM4C123BH6PMI7 (Flash: 256KB).
There was feedback from the "related threads" that it could work without changing…
It is suggesting TM4C123BH6PM for LM3S2965.
But LM3S2965 is 100 Pin IC while TM4C123BH6PM is 64 pin IC.
How is it even the same ?
Please suggest me a TIVA part number for LM3S2965 ( hopefully pincompatible)
Other Parts Discussed in Thread: TM4C123BH6PM Hi all,
I have been using a custom setup that measures 4 channels with the ADCs. I'm triggering both the ADCs with a hardware timer. The main loop is idling in an infinite loop. The chip is TM4C123BH6PM…
Other Parts Discussed in Thread: TM4C123BH6PM , LM117 , INA195 Hi, I'm using TM4C123BH6PM MCU to use a PWM. I'm using this PWM to control my DC motor.
The PWM pulse goes through a motor driver, SI9986.
8875.SI9986.pdf
This is the datasheet of…
Other Parts Discussed in Thread: TM4C123BH6PM I'm using IAR Embedded Workbench for ARM(7.1)
to download my codes to Tiva TM4C123BH6PM MCU using TMS320-XDS100V3.
I've downloaded some example codes from TI Tivaware to test my hardware connection and…
Other Parts Discussed in Thread: TM4C123BH6PM I'm using CCS5.5 to program Tiva TM4C123BH6PM with XDS100V3 Emluator.
I'm trying to make my own function.
The question is that I want to use ASSERT Macro, but I get warnings.
Which header files…
Other Parts Discussed in Thread: TM4C123GH6PM , TM4C123BH6PM , MSP430F135 Hi, I'm using two MCU of Tiva C series which are TM4C123BH6PM, TM4C123GH6PM.
I'm curious of the difference of these two.
(ref : TM4C123BH6PM datasheet page 1271)
Just…