Part Number: TM4C123FH6PM Hi Team,
Customer have observed field failure of thier devci ein field with there crystal.
external 16 MHz crystal and PLL configured for an 80 MHz system clock.
Customer is asking for:
Recommended firmware diagnostics…
Part Number: TM4C123FH6PM With Windows driver provided in TivaWare, we can connect TM4C123FH6PM USB port to PC with Windows OS.
I want to connect TM4C123FH6PM USB port to PC with Ubuntu OS. Let me know whether USB supporting driver availabe for Linux…
Part Number: TM4C123FH6PM Other Parts Discussed in Thread: LP5860 , Is the TM4C123FH6PM SSI port compatible with TI's LP5860 LED Driver SPI Interface? If so, how should the TM4C123FH6PM SSI port be configured (TI synchronous serialinterface?, Freescale…
Part Number: TM4C123FH6PM Tool/software: Our application can update itself and then needs to restart.
The SysCtlReset() call only works when it is executed from privileged mode (f.i. in an interrupt). In order to be able to use it, I would like to trigger…
Part Number: TM4C123FH6PM We are trying to connect keyboard & mouse via hub to the micro-controller.
We found the USB#01 errata, indicating "USB Host Controller may not be Used to Communicate With a Low-Speed Device When Connected Through a hub".
…
Part Number: TM4C123FH6PM in section 23.12.2 of the datasheet it's not clear if VBUS pin (46) will NOT parasitically power the unit. Can you confirm that the unit can NOT be parasitically powered via pin 46 in VBUS detect mode?
Part Number: TM4C123FH6PM Hello,
I need some clarification on the EEprom for the TM4C123x. The datasheet is confusing to me because it uses terminology that is not defined clearly. Our application uses different blocks for different data. Block 0 contains…
Part Number: TM4C123FH6PM Other Parts Discussed in Thread: TM4C1294NCPDT Hello!
I need to make a device which connects to board with CP2102 USB-2-UART bridge on it and communicate to it via virtual UART. I do not see CDC Host functions in usblib, how…
Part Number: TM4C123FH6PM Other Parts Discussed in Thread: SYSBIOS Hi,
I'm working with the Tiva RTOS and I'm having issues debugging the project. Please find below the terminal messages and the ROV information.
The weird thing is that even if I…
Part Number: TM4C123FH6PM Hi team,
MCU Model: TM4C123FH6PM
IDE: CCS8
Tirtos_tivac_2_16_01_14
Xdctools_3_32_00_06_core
The CCS currently in use has been upgraded to CCS10.3, after importing the original project, and compiled, then the automatically…