Part Number: TM4C123GH6ZRB When will the new nFBGA packages be available?
will TM4C123BH6NMRI be drop in replacement (P2P) for TM4C123GH6ZRBI (microstar BGA)?
Thanks!
-Steve
Part Number: TM4C123GH6ZRB
Hello,
I have recently started experiencing some programming failures when working with the TI bootloader loaded in ROM on the TM4C. We have experienced this issue on both the development launchpad board, and with the IC on…
Part Number: TM4C123GH6ZRB I am trying to update code that jumps from a custom bootloader to TI-RTOS. The code gets to the remapped vector table and starts executing code but fails when it starts up tasks. I have read people having issues with the stack…
Part Number: TM4C123GH6ZRB Hello,
I am working with the TM4C123GH6ZRB and am trying to implement a composite device that consists of a BULK interface 0, and a MSC interface 1. Both interfaces work great on their own when they are not in a composite device…
Part Number: TM4C123GH6ZRB We have a product that we are trying to bring new firmware onto. A minimal test product was converted over from a TM4C1237 and now Task_sleep blocks. Worked fine before adjusting the project. Project does use TI-RTOS and driverlb…
Part Number: TM4C123GH6ZRB
Hi fellows,
is there any possibility to change the Microwire Frame Format in a way so that it uses falling edge detection?
I am working on a project where I use the AD9826. The Microwire format works fine for sending but not…
Part Number: TM4C123GH6ZRB Hi Experts,
Good day. Can you help me to identify what's behind suffix "7" for on this two orderable device?
Thank you for your guidance. Regards, Archie A.
Hello Nuno,
So good and bad news though I think you'll primarily find this to be the latter.
The good news is that the USB interface does not seem to have errors associated and my USB analyzer is not picking up any violations of USB protocol nor any…
Part Number: TM4C123GH6ZRB Recently, I have bought a TM4C123GXL LaunchPad.
I realized that there are no CP210x which makes a bridge between USB and UART on the board.
Then, I assume that TI made software bridge between USB and UART in their firmware. …
Part Number: TM4C123GH6ZRB Hello Team,
Quick question regarding the operation of the pwm outputs (ie GPIO_PP0_M0PWM0) during MCU reset (G10, RST*).
Will the outputs become tri-state during MCU reset? This is important because the customer is using the…