Part Number: TM4C129XKCZAD Hello Team,
Customer tested on gpio's toggle speed and the result shows around 400nS high and low period.
May i know the max speed gpio's toggle ?
thanks
Best regards
Part Number: TM4C129XKCZAD I'm going to go ahead and post this because TI is no longer maintaining the USB library or fixing bugs in it, It took me a while to figure out exactly how to fix the bug. There were hints, but no actual fix.
USBHCDPipeWrite…
Part Number: TM4C129XKCZAD I'm writing a host driver that has to send a lot of data from the network to a vendor-specific full-speed device.
My device enumerates, and I can do bulk IN transactions with DMA.
I've been reading up on the existing bugs…
Part Number: TM4C129XKCZAD I'm still mushing along trying to get my USB Host application up and going. I'm trying to transfer a large amount of data to my full-speed device.
I'm setting up a pipe and writing to it in 512-byte work units.
// Output…
Part Number: TM4C129XKCZAD Please will you look at the following clock configuration questions.
1) I want to run the device at 120MHz using the internal PIOSC. I use the following API call:
g_clock_freq_hz = SysCtlClockFreqSet( SYSCTL_OSC_INT | SYSCTL_USE_PLL…
Two things I see. Most important is that the third argument of ADCSequencyDataGet() needs to be a pointer to a 32 bit integer. You are passing ulADC0Value which is an unsigned long.
The second is that since you are running at 120MHz, I think you need…
Part Number: TM4C129XKCZAD Hi,
I am just adding the SSI driver to an application I am developing and the linker complies about the symbol __error__. No other symbol is indicated as "unresolved".
The driver library is properly included:
And the…
Part Number: TM4C129XKCZAD Other Parts Discussed in Thread: TM4C1294NCPDT Tool/software: Code Composer Studio Hi,
I am working on TM4C129X dev board to which I have interface an Power sequencer Ucd via I2C
My aim was to check whether the interface…
Oh, now I understand your question, George. I phrased my case poorly.
What I meant was that I remembered setting some time ago (it turned out to be 2+ years, on an MSP430 project) some enum-related option (which I thought it was on Language options…