Part Number: TM4C129XNCZAD
Hello,
I'm trying to test the UART1 ports with the following code, but it is not working.
Is there anything else to be added or modifed?
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include…
Part Number: TM4C129XNCZAD I'm taking over a project that uses this microcontroller and the instrument has a touch screen, the same one on the development kit board. I have never done touch screen programming before, and the code has lots of functions…
Part Number: TM4C129XNCZAD Dear Sirs:
MCU uses IC " TM4C129XNCZAD", the circuit diagram is attached below.
Now , MCU is not functioning properly,
And Measure the Rbias voltage (Bandgap Voltage Reference) to be 0V.
Is there something wrong with…
Part Number: TM4C129XNCZAD Hello, I would like to add log events in the NDK stack to be displayed in the code composer studio console for debugging purposes. I added the following configurations to the .cfg file: BIOS.logsEnabled = true;
Global.debugAbortLevel…
Hi,
TivaWare_C_Series-2.0 is an extremely old version. In any case, I installed this version and I do not find the directory 'drivers'.
The eeprom.c and eemprom.h files are under driverlib directory. Is it possible your prior colleague made…
Part Number: TM4C129XNCZAD Hello,
I am trying to run a web server hosted on a TM4C129XNCZAD board where the web client sends periodic HTTP requests every 5 seconds to the server.
I used the attached TI example and made a few modifications: - Recommended…
Part Number: TM4C129XNCZAD I've been building my project successfully under another Windows profile. Today IT changed me to a new profile to better fit their policies, and now I'm getting this warning when I build. What could have gone wrong? …
Hi Jean,
Does the error happen after you loaded some program? What is the current program on the flash? It is possible that you can lock out the device if the current program is in some type of deepsleep or hibernate mode without a mechanism to wake…
Part Number: TM4C129XNCZAD Dear Sir,
We are using TM4c129xCZAD design.
In our project we use external interuupt handler to sense -ve edge trigger pulses for frequency 60 KHZ.
The above fast frequency pulse are input to the controller two diffrent pin…