Hey Neet,
The TMAG5111 uses the same circuitry as the TMAG5110. If you look at figure 8-3 in the datasheet, you can observe for the TMAG5110 that there are two sensors monitoring the flux in two perpendicular axes (90° out off phase). Based on the…
I will look into the data more closely.
I have been able to source some different multi pole and diametric targets that fit my system. Can I use the TMAG5170 with multipole or am I better of the diametric?
Using a pair of TMAG5110 or TMAG5111, would either…
Other Parts Discussed in Thread: TMAG5110 , TMAG5111 Looking for the 2-d hall sensor with analog output(linear) at 30000 rpm.
Similar to: https://ams.com/documents/20143/4387125/AS5116_DS000686_4-00.pdf
https://ams.com/documents/20143/4387125/AS5116_DS000686_4…
Other Parts Discussed in Thread: LDC3114 , TMAG5110 , TMAG5111 , DRV5013 , DRV5023 , TMAG5123 , DRV5033 , TMAG5124 Hi,
Here are the details of Digital Input – Sensing requirement (Isolation not required).
Input voltage range 0V to 16V DC
Active – High…
Part Number: TMAG5170-Q1 Other Parts Discussed in Thread: DRV5055 , TMAG5170 , TMAG5110 , TMAG5111
Is TMAG5055 capable to use like encoder? Can it detect changing magnetic field at 10000rpm? (if the magnetic field is within the sensor limit)
The sensor is…
Other Parts Discussed in Thread: TMAG5110 , TMAG5111 , TMAG5170 , TMAG5273 Hi all
I'm looking for a magnetic sensor which should be a industrial grade and it should be able to determine the speed and RPM of the motor in the industry.
I'm not able to find…
Part Number: DRV5056-Q1 Other Parts Discussed in Thread: TMAG5110 , TMAG5111 , TMAG5110-5111EVM , DRV5055 , TMAG5170 , TMAG5273 , DRV5032
I need help in choosing a hall effect sensor. The application is to detect the revolution and direction of the wheel. I…