Part Number: DRV5011 Other Parts Discussed in Thread: TMAG5110 , TMAG5111 We are developing a product for condition monitoring (Predictive maintenance ) of motor, We intend to measure the speed of the three-phase induction motor just by mounting the wireless…
Part Number: TMCS1108 Other Parts Discussed in Thread: TMAG5110 , TMAG5111 , TMAG5170 , TMAG5273 Dear Team,
Does we have any solution have linear optical scale function as below?
(MU150)
Many thanks,
Jimmy
Other Parts Discussed in Thread: TMAG5110 , TMAG5111 , DRV5032 I need to get the speed of an e-scooter and display it on an LCD screen together with battery level and light ON/OFF. Which hall sensor or optical sensor can be used to detect speed of the moving…
Part Number: DRV5011 Other Parts Discussed in Thread: TMAG5110 Hi,
I want to use DRV5011 TO-92 Package. I found the footprint details from datasheet. I'm little confused with the number direction from this image.
Can anybody help me. Is this bottom…
Sayali,
Unfortunately, the only Hall Effect latches we currently offer in the X2SON package are DRV5011 and DRV5012.
DRV5013, TMAG5110, and TMAG5111 are all capable of operating up to 38V, but these devices are all offered in either SOT23 or TO92.
Thank…
Hello user,
We dont have an exact replacement here and can provide some information on alternative parts and technologies... Have you had a chance to look at our portfolio of Hall sensing devices ? We have recently released Hall sensing latch TMAG511…
Sergey,
Sorry for the delayed response. It was a holiday weekend for us.
You are right. If the device loses power within the hysteresis range, it will not retain the latched output since the input could be less than the operating threshold but still greater…