I download and install Graphics_SDK_4_05_00_03 on my beagleboard.
Build it with xorg support.
And I see that almost every application that uses GTK+/X11 or Qt/X11 show garbage instead of letters.
So I dig into this, and write simple application…
Part Number: LPSTK-CC1352R Other Parts Discussed in Thread: UNIFLASH , CC1352R
Setup:
SDK: simplelink_cc13x2_26x2_sdk_5_10_00_48 Compiler: CCS Compiler Uniflash: 6.3.0.3193 Programmer: TI CC1352R LAUNCHXL and Segger Devices: Two CC1352R LPSTK revision…
Part Number: AM5728 Tool/software: Linux On the AM5728evm board, once the Wayland/weston is stopped, the second crtc and encoder is not initialized. And though we can not use HDMI connector any more.
Is there any example code to initialize them by calling…
Hi David,
I'm including the ADS1x18EVM user's guide in this post. This should be available on the web tools page soon.
sbau357.pdf
Have you been successful in getting the GUI to work with the EVM? Were any of my suggestions helpful?
Best regards…
Hi Tyler,
I have attached a guide that seeks to document the intrinsic commands of the HCI tester scripting language
/cfs-file/__key/communityserver-discussions-components-files/538/HCITester-Quick-Reference.pdf
>> I know the software is given…
Hi Jared !
As you know the yocto-build of tisdk-edgeai-image (v9.1.0) was completed successfully, hence I tried to flash the .wic.xz file on sdcard.
Following methods I have tried:
Flashing the .wic.xz file using Balena etcher
Flashing the …
Hello,
My name's Zach, and I work at a start-up called Spark. We sell an open source development kit based on the CC3000 (paired with an STM32 microcontroller) called the Spark Core. We have shipped more than 10,000 CC3000 development kits around the…
Hi,
I've looked in the example,
at <NDK_INSTALL_DIR>\packages\ti\ndk\tools\console\contest.
Seems that I'm doing all OK. However problem still persist....
Please note that my tasks for transmit message via LAN (child socket are static and not…
Part Number: ISO5452 Other Parts Discussed in Thread: ISO5451
Hi,
The attachment is the IGBT I used. I didn’t understand very well when designing the ISO5452 pin 2 Desat function, so please help:
1. D4 design considerations, how many volts do I…
Other Parts Discussed in Thread: SYSBIOS Dear all:
on page 7th of DM814x_EZ_Software_Developers_Guide.gdf , i know the codec engine examples can not be run out with graphics,so i execute "/etc/init.d/load-hd-firmware.sh stop " , the codec engine application…