Part Number: TCAL9539-Q1 Other Parts Discussed in Thread: TMAG5173-Q1 , , TCAL9539
Tool/software:
Hello,
We are using multiple TMAG5173-Q1 and a single TCAL9539-Q1 IC on the same I2C bus in our project. If we start the measurement simultaneously…
Part Number: TMAG5173-Q1 Tool/software: Hello,
I am testing this sensor for AFE CHECK.
The execution time is 200us according to safety manual. But I get wrong result in that time. I need to wait at least 500us to complete conversion and get correct…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TCAL9539-Q1 , TCAL9539
Tool/software:
Hello,
We are using multiple TMAG5173-Q1 and a single TCAL9539-Q1 IC on the same I2C bus in our project. If we start the measurement simultaneously on…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5170 Tool/software: Hi team,
I would like to ask something about the output result of TMAG5173A2 with the TIMSS tool. From the datasheet, I think when the magnetic is 266mT, the output of…
Part Number: TMAG5173-Q1 Tool/software: Hello,
I just found a very important change on the data sheet for this part. In the past, the September 2022 version of the datasheet for the device, there was a "wake and sleep" mode for this device. Now when…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5170 , , TMAG5170-Q1 Hi,
435 / 5,000
I am preparing to use a 3D Hall effect sensor = comparing TMAG5173 and TMAG5170…
Part Number: TMAG5173-Q1 Tool/software: Hello,
We want to make hall effect push buttons with s afety compliant . I have tried this sensor and my measurements are:
-09 mT when not pressed
-27 mT when pressed
Is it suitable for push button application…
Part Number: TMAG5173-Q1 Tool/software: Hello,
I am working with two Hall sensors that I read alternately over I2C. I am only measuring the Y and Z axes with 8-bit resolution, and CRC is enabled. As a result, I receive 4 bytes per message. The sensor…
Part Number: TMAG5173-Q1 Tool/software: I'm looking at the data sheet and see "The threshold value in mT is calculated for A2 as (133(1+X_Y_RANGE)/128)*X_THR_CONFIG". If I am reading this right that would mean if I put a value of 1 into the 8 bit register…
Part Number: TMAG5173-Q1 Hi Team,
My customer used TMAG5173-Q1 to develop the HMI. I'm not familiar with the part.
Do we need to do initial setting for 0h-Bh register before getting result from 10h-1Ch?I
If so, do we have initial setting script…