Part Number: BQ25798 Other Parts Discussed in Thread: BQ24133 Tool/software: Hi,
I use a BQ25798 with adapter and 1S battery. The VPMID is configured to be 7V.
The usercase is that the device works on battery (without adapter). This case works well …
Part Number: DRV8329AEVM Other Parts Discussed in Thread: LAUNCHXL-F280049C Tool/software: I am using the DRV8329A EVM with the TMSF280025C LaunchPad and running the Universal Lab Project . I want to tune a different PMSM motor that is not included in…
Hi Roy, There are some sample wav files in asdk-10.00.00/ti-asdk-bsp/packages/dspc/a53/AWECore/Audio/ folder. You can try these for now. Regards, Ritapravo
I have replaced TPS with TPS25751, and it now works as expected thanks to your advice. Regarding the previous issue with RE: TPS25750: non-PD adapter after first connection latched BQ25713 that no usb connection can charge there is new problem of charge…
Part Number: MCF8329A Other Parts Discussed in Thread: MOTORSTUDIO Tool/software: Hi,
Actually I need to redesign the existing MCF8329A EVM. Since i had a application that requires around 90 A to run the motor. As of now the existing design is suits…
Hi Chen,
Even if the received frame is less by a byte, this error would be printed. So again, please check the size in the CSIRX and what is received from the sensor. They should exactly match.
and since you are only receiving 2 frames, this print also…
Hi Bhatt
I am unable to upload my code; there might be an issue with this forum.
First, I observed that this situation only occurs with this particular function. My code contains assembly instructions, and when I remove the assembly line shown in the image…
Hi Simon,
Thanks for the update. That is correct, using the wrong configuration with the EVM could lead to issues. Is the EVM working properly with adapters now?
I would recommend reviewing the Liquid Detection setup section of the TPS25751EVM user guide…