Part Number: TMDS1204 Other Parts Discussed in Thread: TDP1204 I am trying to output TMDS/FRL signals by applying an HDMI IP to an FPGA.
But due to the characteristics of the FPGA GT (GPIO out), it only supports a 0 to 800mV swing without a common-mode…
Part Number: TMDS1204 Hi,
I'm using the TMDS1204 (fan-out buffer feature enabled, HDMI 1.4/2.0 mode, RCLKOUTp/n active) and want to AC-couple RCLKOUTp/n into a third-party CML fanout buffer (Micrel/Microchip SY58011U) for clock distribution.
The datasheet…
Part Number: TMDS1204 Tool/software: Hi Team, I am using TMDS1204RNQR Retimer IC in my project. And my FPGA supports like when the Cable detect (Rx detect) should go first from the Source (Laptop) to the retimer IC to the SOC using HDMI RX connector.…
Part Number: TMDS1204 Hi Team,
We are using the TMDS1204RNQR IC for HDMI 2.1 validation . Currently, we are configuring the device using the pin-strapping method for both HDMI TX and RX .
We would like to understand how to verify through software…
Part Number: TMDS1204 HI
We are using HDMI redriver TMDS1204RNQR in our Versal (XCVE2302-1LSISFVA784) based design.The HDMI display pipeline initializes successfully, the monitor is detected via EDID, and the DRM pipeline is configured without errors…
Part Number: TMDS1204 Tool/software: I am having one query regarding TMDS1204 IC, refer below image, in that i am seeing one MUX functionality internally there in the redriver IC, in that MUX toFPGA connection, FRL data pin and the RCLKPin is connected…
Part Number: TMDS1204 Tool/software: As per TMDS1204 datasheet, the ESD part mentioned is PUSB3FR4 IC. In this IC, i have connected the Data lines and clock lines which is going to GPU and HDMI TX connector. Only 4 channels are available in this ESD IC…
Part Number: TMDS1204 Tool/software: Hi David, This IC TMDS1204 can support as HDMI 2.0 version also, now my design is implemented same like HDMI 2.1 as per the reference design mentioned in the datasheet., In future, if i want to change the HDMI Version…
Part Number: TMDS1204 Tool/software: For HPD IN signal, for sink application, if i used level translator to convert the HPD_IN signal from 5V to 3.3V using inbuilt level shifter and can use HPD_OUT signal as 3.3V IO level and using one level shifter externally…
Part Number: TMDS1204 Tool/software: We designed an HDMI input/output board using a combination of the TMDS1204 and an AMD FPGA. The HDMI compliance test was conducted by the HDMI certification body and the following FAILs were noted.
Please let me…