Part Number: TMDS171 Dear All,
Would you kindly tell us the recommended treatment for the SCL_CTL and SDA_CTL pins of the TMDS171 when using the TMDS171 in "Pin Strap mode" with I2C_EN set to low(I2C_EN/PIN = Low)? Is it okay to pull up the SCL_CTL…
Part Number: TMDS171 Hi All,
Please kindly tell me "Table 7. CSR Bit Field Definitions, REV _ID (08h)" in "8.5.3 CSR Bit Field Definitions, REV _ID (offset: 00001000) (reset: 01h)" contents. I think that this 08h register should normally read 01h in…
Part Number: TMDS171 Tool/software: Hello,
my name is Roberto Teodori and I need a clarification about one of the features listed in the TMDS171/I Datasheet.
I' m referring to Inter-Pair Skew Compensation of 5+ Bits.
5+ Bits means that skew compensation…
Part Number: TMDS171 Other Parts Discussed in Thread: SN65DP149 , Tool/software: Hi All,
I have a question about the TMDS171 and SN65DP149.
Do I have to input HDMI TMDS data0+/- to the TMDS171's IN_D0p/n terminal? For example, I think it's fine to…
Part Number: TMDS171 Other Parts Discussed in Thread: SN65DP149 , Tool/software: Hi All,
I have a question about TMDS171 and SN65DP149.
Is it possible to input negative to D2p and positive input to D2n as shown in the figure below?
Since it is…
Part Number: TMDS171
Hi team
We use Linux platform to develop our product, and has a TMDS171 on our board for HDMI.
I have the following questions that need your help:
1. Does TMDS171 has a Linux driver to control the power-on sequence ?
2…
Part Number: TMDS171 Tool/software: Hi All,
I would like to send and receive TMDS signals (DVI signals) via SFP+ using TMDS171IRGZT. The other side is CML, so do I need a conversion bridge IC between CML and TMDS? In this case, it may be possible to…
Part Number: TMDS171 Dear Expert
We would like to consult TI about automatic EQ. Is there any EQ with a 14dB higher EQ capability than TMDS171?
The customer needs to support a 20m DVI cable, preferably up to 30m.
Part Number: TMDS171 Tool/software: Hi,
Our host processor supports only MIPI CSI-2 interfaces. But the system input is DVI. Can you suggest best solution to convert DVI to MIPI CSI-2?
Regards,
Vijetha HN
Part Number: TMDS171 Other Parts Discussed in Thread: TDP0604 Tool/software: Hi All,
Customer is currently using TMDS171. The DVI output waveform is not very good. Are there any devices that can improve the waveform quality? Please recommend some redriver…