Part Number: TMDS181 Other Parts Discussed in Thread: TMDS171 , Hi
Please help to check and advise TMDS171IRGZT is replaced by TMDS181IRGZR Does the hardware schematic need to be adjusted or modified?
6281.TMDS171.pdf
Part Number: TMDS171RGZEVM Other Parts Discussed in Thread: TMDS171 Hi team
I have a question. I am planning to use EYESCAN to check the eye pattern of TMDS in TMDS171RGZEVM.
Is the result displayed by EYESCAN the input pattern of TMDS171? Or is it the…
Part Number: TMDS171 Hi Team,
My customer wants to swap TMDS signal lines in front of display input. Does TMDS171 support reverse polarity connection on output side as well as below? In my understanding, there is no issue in such the use case since TMDS171…
Part Number: TMDS171 Hı Team,
Can you please check and advise with following request:
"
Can we learn the maximum junction temperature values for TMDS171I?
"
Thanks in advance
Best Regards
Furkan Sefiloglu
Part Number: TMDS171 Other Parts Discussed in Thread: TMDS181 , Hi,
To support DC-coupled HDMI input (with HDMI output) of redriver, is TMDS171 or TMDS181 the only solution from TI (as a retimer)? Is there any other option?
Thanks,
Antony
Part Number: TMDS171 Hi team,
Which power rail should be powered up first, VDD or VCC?
Figure 23 is confusing, because it seems that there are not restriction.
And there is the description like below in the datasheet. Does this mean they don't need…
Part Number: TMDS171 Hi, dear TI!
I read in the datasheet on TMDS171 in table 36 that with OE = 'L' I2C is off.
My Q: If I have multiple TMDS171 on the board on the same I2C bus, but only one is active at a time, won't the others (disabled) TMDS171…
Part Number: TMDS171
Greetings,
i would like to ask if it's possible to know how the TMDS171 produces the data for the eye diagrams shown on the EyeScan tool software.
Are there any particular registers on the TMDS171 or formulas that can be used…
Part Number: TMDS171 Hello team, My customer has a question about DDC-SCL behavior. He is use TMDS171 as source side application as below. When 400kHz clock input from DDC -SCL_SRC, he saw that 74.20kHz clock from DDC -SCL_SNK. It seems that TMDS171 ACTIVE…