Part Number: TMDS181 Hi Team
My customer Lango need a IC, which called HDMI 2.9 Splitter, below are some specs, I haven't support such products before, so could you please provide the path to search the related ics or there are some solution in TI which…
Part Number: TMDS181 Dears:
The picture shows two connection modes of DDC circut
Paranormal:The display appears unusually at 4k@60hz resolution,When DDC circuit in accordance with Figure 1;
But the display appears normally at 4k@60hz resolution,When DDC…
Part Number: TMDS181 Dear Sir
We're doing a stress test. The relay was used to realize 5S hot swap, but no output signal was found. It is checked that HPD_SRC has input 3.3V signal, but HPD_SNK has no output 3.3V signal. The HDMI connection cannot detect…
Part Number: TMDS181 Hi,
I'm designing in the TMDS181 as an HDMI sink and I was wondering if my schematic can be reviewed and the following questions answered:
I have the DDC I2C pulled to 5V on the connector side. The SCL_SNK/SDA_SINK go to 3.3V…
Part Number: TMDS181 Hi Team,
Can you help answer the problems? Thanks.
1. What does the silkscreen on the IC mean?
2. Storage conditions and valid storage dates.
3. Detailed RoHS report.
4. A complete list of reliability test items.
5. The detailed soldering…
Part Number: TMDS181 Hi Team
My customer is using TMDS181 in their HDMI 2.1 application and reported compliance test failure due to the low impedance.
The test they used was №HF2-4(Sink TMDS Electrical – 6G – Differential Impedance),
where…
Part Number: TMDS181 Hi team,
Customer need AC coupling for output, but in FPGA side, there has been already pull-up resistors. But I know that in TMDS181 side, it also requires pull-up resistors. I was wondering if you could give some advice on whether…
Part Number: TMDS181 Hi Team,
According to the DS of TMDS181IRGZR, the maximum time of VDD stable before VCC is only 200µs.
However, the delay time and soft-start time of the Vcc power regulator is over 200us. Please reference the waveform below…
Part Number: TMDS181 Hello Team,
The TMDS181 allows TX and RX to be reconfigured using the apply_RXTX_changes register. Does it need to update the Clock Ratio Status etc. when using this register? We want to use the TMDS181 in the source application…