Part Number: TMDS181 Hi all. Curious if anyone has run into this similar issue failing Voff compliance test measurements on the data lines using the TMDS181 with the Keysight DSAV164A. For other video sources with no TMDS181, this test passes fine with…
Part Number: TMDS181 Hi everyone,
Following the datasheets of the COM Express module and the MXM GPU board we have to place DC blocking capacitors for HDMI applicationon the baseboard.
We have a retimer based on TMDS181.
Where do we insert the capacitors…
Part Number: TMDS181
Hi.
This is a question related to TMDS181. I have configured the circuit using TMDS 181, and HPD HDCP works normally, but the TMDS channel does not seem to work.
I'm not sure if it's a circuit configuration mistake, so please check…
Part Number: TMDS181 Other Parts Discussed in Thread: SN75DP159
Hi Team,
Could you pls help check if TMDS181 is the best option to replace PS8419, which is used for HDMI 2.0 port of the all in one? And I am wondering two or one devices are needed for…
Part Number: TMDS181 Hi team,
We are considering using the TMDS181 in ReTimer mode with a data rate of 1.48Gbps. I would like to know the following two points about above operation condition.
1.1.48Gbps input mask opening value In Figure 13 (Input Eye…
Part Number: TMDS181 Why would one not want to use mode retimer mode across full range 250 Mbps to 6 Gpbs? I was surprised this is not the default setting. So, it got me curious if we need to be concerned running this in this mode all the time? Because…
Part Number: TMDS181 Other Parts Discussed in Thread: SN75DP159 , , Hello,
We are observing an issue with specific video source 1080p60 (camera) when using SN75DP159 device on sink side.
We can replicate this issue on TMDS181RGZEVM eval board:
Source (camera…