Part Number: TMDS181 Why would one not want to use mode retimer mode across full range 250 Mbps to 6 Gpbs? I was surprised this is not the default setting. So, it got me curious if we need to be concerned running this in this mode all the time? Because…
Part Number: TMDS181 Other Parts Discussed in Thread: SN75DP159 , , Hello,
We are observing an issue with specific video source 1080p60 (camera) when using SN75DP159 device on sink side.
We can replicate this issue on TMDS181RGZEVM eval board:
Source (camera…
Part Number: TMDS181 Hi everyone,
I noticed that there are no more capacitors 0.1UF on the differential pairs whatever they are on the input or the output.
Is it OK ?
Best regards,
Michel
Part Number: TMDS181 Other Parts Discussed in Thread: TFP403 , TMDS171 , DS34RT5110 Hi TI
We are looking for HDMI 1 to 2 solutions, port A to TFP403 and port B to the next stage. Does TI have solution for my application? or TMDS181 and PI3HDX412BD as below…
Hi,
You can refer to this section in the TMDS181 datasheet. But they have two HDMI switches between the TMDS181 and the HDMI2.0B. Are these passive switches? Does the HDMI2.0B have any skew compensation to compensate the skew, the insertion loss, etc between…
Part Number: TMDS181 Dear Support team,
We want to apply TMDS181 as repeater.
Do you have any application note or block diagram for repeater use case?
We want the similar document and block diagram like "Figure 35. TMDS181 in Sink Side Application" in…
Part Number: TMDS181 I see we can use pin strapping and can have TX_TERM_CTL set to no connect where the device automatically selects the termination impedance. We are considering using I2C mode instead and assume there is some way we can programmatically…
Part Number: TMDS181 If we use pin strapping, I understand we can still do I2C reads. But if we set EQ_SEL/A0 to no connect for adaptive eq, what is the state of A0 for the I2C address? Because we are not pulling up or down EQ_SEL/A0, I was not sure if…
Part Number: TMDS181 Hi Team,
Customer met an issue when using TMDS181 and hope you could help~
Connection: 4K source - TMDS181 - FPGA
Customer found that its BERT error count shows some error happened in device. And according to datasheet, BERT error…