Part Number: TMS570LS1227 Other Parts Discussed in Thread: TMDS570LS12HDK Hi,
My custormer have one hercules EVM the part number is TMDS570LS12HDK.
When I try to download bellow user's guide and sample code. The ti-wiki website show my IP or email has…
Hi Ju We,
We don't have any specific PCB layout guidelines documentation.
It would be better to use the HDK PCB layout files as reference.
You can download them from below link:
TMDS570LS12HDK Development kit | TI.com
Once you download and extract…
Part Number: TMS570LS1114 Other Parts Discussed in Thread: SAFETI-HALCOGEN-CSP , HALCOGEN Hello TI support,
We are trying to execute SAFETI-HALCOGEN-CSP for TMS570LS1114 and for that we purchased LDRA-Unit for TI, but after following all the steps defined…
Hi Yash,
I tested without transceivers and found it is not working.
Only two transceivers are fine, one for CAN1 signals and other for CAN2 signals, like shown in below pic
For more details refer design files in below HDK board link
TMDS570LS12HDK Development…
Other Parts Discussed in Thread: TMDS570LS12HDK I'm developing software for a custom PCB using the TMS570LS1114PGE, a XDS200 debugger, and Code Composer 6.1.2.00015. The board schematic for the JTAG interface is based on the TMDS570LS12HDK, which I…
Other Parts Discussed in Thread: TMDS570LS12HDK , HALCOGEN Jean-Marc this is great and runs well on my TMDS570LS12HDK but it there an example showing how to do just a simple SPI slave without the DMA? The DMA just seems like magic and all I want to do is…
Hi Fabian,
Did you get the example up and working? A am currently working on setting up a Flexray network between two TMDS570LS12HDK and could use some help here.
Best regards
Hi again Anthony,
So as i understand it now, the expansion board you linked to works with the TMDS570LS12HDK? Otherwise I could also build the expansion board and jump the wires/ adapt it to fit with the LAUNCHXL2-570LC43?
Again, thank you so much…
Other Parts Discussed in Thread: TMDS570LS12HDK Hi
I try to run CCS on a Windows 8.1 in VMWare Fusion on OS X 10.10.5. (MacBookPro 15", Mid 2014)
I tried to debug a simple project on several different HDK's (TMDS570LS12HDK, XDS100v2). Programming…
Yes, the Q4 is the hottest of the four on both boards. It's a gradient. If Q4 is 84F, then Q3 is 80F, Q2 is 76F, and Q1 is 72F.
MCU is:
connected with jumpers.
DRV8711 is powered by two bench-top power supplies (one for 27V, one for 3.3V).
Current…