Hello,
Several functions are multiplexed on this microcontroller. For example N2HET1[8] is multiplexed with MIBSPI1SIMO[1], MII_TXD[3], and USB1.OverCurrent on ball E18. To use E18 as N2HET1[8], 0x01 should be written to PINMMR14[7:0].
On HDK board…
Hello QJ,
Many thanks for your help. I will do it after my careful consideration with worry of my shaky modification. Is it possible to use TMDS570LS31HDK without any modification ?
Best regards
Datïan
Part Number: TMDS570LS31HDK If the ERROR pin going low is not used by an external unit to reset the processor there appears to be a gap in the handling of :
FMC uncorrectable error - Bus 2 accesses [not address parity or EEPROM bank accesses]
The…
Hello,
The CPU must be in a privileged mode to write to this register in the interrupt manager. Please refer to this app note for details on the operating modes and for methods to switch modes.
www.ti.com/.../spna218.pdf
Regards,
Sunil
Attached is the log for the Debug and Release versions. Thanks.
CCS 6.0.1.0040 kit is TMDS570LS31HDK (2014 vintage) TMS570LS3x_demo_software.build.log TMS570LS3x_demo_software.build.log
Part Number: TMDS570LS31HDK The VIM RAM is initialised with parity and both the ISR and the parity parts are set up ok.
When FBPARERR is given an ISR address and a parity error created in VIM RAM parity 0xFFF82400 , the ISR is continually re-entered…
Part Number: TMDS570LS31HDK
I have the TMDS570LS31HDK. In the board the chip that is used is the TMS570LS 3137DZWTQQI YFD-69APLFW.
Creating a new HALOCGEN project which software packet have I to use?
The devices that I can select are shown on the…