Hi Santosh,
As AUTOSAR does not have specific requirements w.r.o PWM outputs per channel, MCAL PWM driver is designed to update duty cycle same for both outputs.
So if duty cycle is changed on OUTPUT A, it will be applicable to OUTPUT B as well. It cannot…
Part Number: TMDSCNCD263 Hi.,
I am using the SDK mcu_plus_sdk_am263x_08_06_00_34. I try the Example Code uart_echo_dma_am263x-cc_r5fss0-0_nortos_ti-arm-clang I Change Read & Write Transfer Mode to Callback. Then I Write Tx and RX
in While loop Once…
Part Number: TMDSCNCD263 Hello Team,
I have an issue with Shared Memory section allocation.
Map file is showing expected address of the memory section.
But when i load the symbols, address of the memory section is changing compared to MAP file.
*When…
Part Number: TMDSCNCD263 I have a TMDSCNCD263 controlCard, CCS v12 is in Linux, when I was trying to download binary today, it says there is an update for the XDS110 driver, I entered yes. after it came back, no way to connect o to the target.
is there…
Part Number: TMDSCNCD263 Other Parts Discussed in Thread: UNIFLASH Hi.,
I try Sbl can uniflash. I try the procedure mention in the below link. Application flashing sequence is completed. Application not working after restart the board.
software-dl.ti.com…
Part Number: TMDSCNCD263 Other Parts Discussed in Thread: AM2634 Hello Team,
we are using CAN driver from MCAL_AM263x_09.00.01.00 package, we are trying to create autosar CAN stack with both CANFD and CAN feature together on same MCAN1 channel bus of A…
Part Number: TMDSCNCD263 Other Parts Discussed in Thread: UNIFLASH , AWR1843BOOST , AM2634 Hello Team,
I am working for a bootloader project.
Currently, bootloader is loaded into RAM using CCS.
Now i would like to flash bootloader into external flash using…
Part Number: TMDSCNCD263 The issue is related to E2 version AM263x Control Card.
I am using this CC to validate one TIDM design. I am giving +5V supply to the design and seeing LD16 LED on the CC board is glowing red. This causing JTAG failure. I am using…