Part Number: TMDX5505EZDSP Hello Team,
My customer is looking for the design files/schematic of the TMDX5505EZDSP, is this possible to be shared with them? Also can you provide the power consumption of the device?
Regards, Renan
Part Number: TMDX5505EZDSP Hi there,
I wanted to get clarification from a TI rep before purchasing this part. Our project will need to access the I2S and SPI interface lines and we were wondering if this is possible when interfacing with the Expansion…
Part Number: TMDX5505EZDSP Problem connecting to the board (C5505 eZdsp).
Full error reads:
Error connecting to the target: (Error -1143 @ 0x5F) Device core was hung. The debugger has forced the device to a ready state and recovered debug control, but your…
Part Number: TMDX5505EZDSP Tool/software: Code Composer Studio Hi,
I have a project to make, using the C5505 eZdsp USB Stick to output the input audio but every sample needs to be reversed, if the sample is "1" the output to sample needs to be "-1"…
can i debug this TMDX5505EZDSP with its usb only or do i need separate JTAG connection..they have mentioned that TMDX5505EZDSP tool has embedded XDS510 emulator for full source level debug capability...what does it mean exactly ..?how i m going to debug…
Part Number: TMDX5505EZDSP hi,
Is there any specific Microphone that needs to be used for Stereo IN port in USB STICK VC
5505 (Rev B). We are facing issues like, when we give audio data from Mobile the Stereo IN
port is working fine, where as if use…
Part Number: TMDX5505EZDSP Hi Team,
One of our customer is using TLV320AIC3204 and want to know weather a normal PC MIC is compatible with this CODEC TLV320AIC3204 . They are evaluating ezDSP USBSTICK C5505 : Rev D EVM and using standard PC mic and not…
Part Number: TMDX5505EZDSP Tool/software: Code Composer Studio Hello,
I just unpacked a new TMS320C5505 eZdsp stick for a class and I'm having trouble connecting and even running the basic Hello World example.
I'm using CCS version 7 (newly downloaded…
Part Number: TMDX5505EZDSP Tool/software: Code Composer Studio Hi folks,
I just started to work with EZDSP USB STICK C5505 under CCSV7. Everything works fine, except i can't figure out how to create a launcher that download and run the binary, without…
Part Number: TMDX5505EZDSP Hello,
I'm using the C5505 eZdsp USB stick development tool with CCS version 7. Sadly, all the information I can find online to setup the device uses version 4 or 5, which do not run on Windows 10 (which I'm using). So the tutorials…