Part Number: TMDXIDK5718
I downloaded "ti-processor-sdk-linux-am57xx-evm-06.03.00.106-Linux-x86-Install.bin" to set up TMDXIDK5718. The setup process went successfully, except for board setup part. The board was detected correctly on /dev/ttyUSB1…
Part Number: TMDXIDK5718 Up to this point, I have been able to generate a custom version of tisdk-base-image wic file which I burned an sd card which boots successfully. Now, I'd like to implement network booting with the custom build. I can locate…
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: AM5718 ,
My question is regarding am5718 and its eval board TMDXIDK5718. I'd like to (try to) use Linux Mint 21.1 instead of Ubuntu 18.4 as host Linux system and set up the SDK on it. When I…
Part Number: TMDXIDK5718 Hi.
Is there a document that describes how to use the Linux test suite under /opt/ltp? I'd like to exercise various interfaces available on TMDXIDK5718.
Thanks.
Peter
Part Number: TMDXIDK5718
Hello,
I'm trying to build SDK, but i get this error:
user@user-HP-Z420-Workstation:~/ti-processor-sdk-linux-am57xx-evm-08_02_01_00/yocto-build/build$ MACHINE=am57xx-evm bitbake -k tisdk-default-image
ERROR: Unable to start…
Part Number: TMDXIDK5718 Hello,
I am working with the TMDXIDK5718 board, using SBL to boot an image from an SD card. It was working correctly until suddenly failing with this error received over serial:
So far I have tried:
Replacing the MLO and app…
Part Number: TMDXIDK5718 Hello,
I'm currently using the PRU ICSS EtherCAT Slave provided by Texas Instruments on a AM57x Sitara board. The provided firmware flashes a Frame_Handler firmware to PRU IRAM0 and Host_Interface firmware to PRU IRAM1. For…