Part Number: ADS1258 Other Parts Discussed in Thread: TMP235 , We have data acquisition boards each running 9 x ADS1258 in continuous conversion mode across 16 channels.
Our boards performed without issue for a few weeks running 24x7 at slightly elevated…
Dear Josh,
thanks a lot for your help! I got your point - sounds logical :)
Another short question here. Actually, I use already the TMP235 sensor in my project. And I am considering now to have the different redundant sensor with different output gain…
Part Number: LM35 Other Parts Discussed in Thread: TMP235 Team,
-The LM35 datasheet is not well organized to understand which variants are the subset of which one.
Could you please summarize what LM35 variants can be replace which one in term of temperature…
Is the "TS_EN" (J9) jumper installed? That powers the TMP235 Temperature Sensor, which feeds P1.1 [Ref LP UG (SLAU802) Fig 19].
I expect if you remove that jumper the TMP235 won't interfere. Alternatively, try using (e.g.) P1.7 (A7), which doesn…
Thank you, Jalen.
Do you have any testing data to back up the "Most likely the LM50-Q1 will continue to follow the 10mV/°C" comment?
I will propose TMP235-Q1, however, it's pretty late in the design cycle, and I am not sure they will be able…
Part Number: TMP411 Other Parts Discussed in Thread: TMP451 , TMP461 , TMP1075 , TMP235 Hi sir,
I am planning to use the TMP411 temperature sensor for my design to measure the temperature of a clock synthesizer.
Since the clock IC doesnt have dedicated temperature…
Part Number: LM335A Other Parts Discussed in Thread: TMP235-Q1 , LM45 , LM50-Q1 , LM61 , LMT90 , LM50 , TMP235 Can you recommend a similar style device that comes in a smaller SMT package? SOT-23, SC-70, etc. SO-8 is pretty big, TO-92 is big and thru hole.
…
Other Parts Discussed in Thread: TMP112 , TMP116 , LMT01 , TMP235 , TMP61 , TMP63 , TMP64 What should I consider when choosing a sensor to measure ambient temperature?
Hi Jonathan,
The internal temperature sensor is transistor based like our analog output temperature sensors (TMP235, for example.) It's not affected by bias voltage like a thermistor would be.
Has the customer set the correct OP_MODE (page 23) for…